2017-05-08 5:48 AM
Hi,
I have the STM32F479I-Eval Board and OV5640 Camera Module running with a modify code of STM32469I_EVAL\Applications\Camera\Camera_To_USBDisk. I can save pictures in JPG format at 640x480,1280x720,1280x960,1920x1080, but when i try save pictures in 2592x1944 it doesn't work.
I read [RM0386(16.6.1)] -> maximum input size is 2048 × 2048.
Could this be the cause?
Any idea how to fix it?
Someone has this camera working in JPG format at 5 Megapixels?
Best Regards,
Sergio
2017-05-08 7:07 AM
>>maximum input size is 2048 × 2048.
Could this be the cause?
Look at the registers implicated, and if they only hold 11-bits. ie write a maximal value, and check if high order bits remain zero.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.