2024-07-18 4:32 AM - last edited on 2024-07-18 4:39 AM by mƎALLEm
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1,1000);
readValue1 = HAL_ADC_GetValue(&hadc1);
HAL_ADC_Stop(&hadc1);
HAL_Delay(100);
HAL_ADC_Start(&hadc2);
HAL_ADC_PollForConversion(&hadc2,1000);
readValue2 = HAL_ADC_GetValue(&hadc2);
HAL_ADC_Stop(&hadc2);
HAL_Delay(100);
HAL_ADC_Start(&hadc3);
HAL_ADC_PollForConversion(&hadc3,1000);
readValue3 = HAL_ADC_GetValue(&hadc3);
HAL_ADC_Stop(&hadc3);
HAL_Delay(100);
after executing this adc code the read values of readValue1, readValue2 and readValue3
are mutually reading the same value. i.e when i try to change the adc value of readValue3 with pot the other values are also changing
need help here...
thank you.
2024-07-18 4:38 AM
Hello,
I invite you to read the tips on how to post a thread in this community as you are not following our recommendations in posting especially the title and the the code sharing.
So could you please edit your post according to these recommendations?
2024-07-18 5:55 AM
Show your ADC setup. Nothing wrong in the code you posted. Are the ADCs perhaps all looking at the same channel?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.