2013-10-16 9:37 AM
STM32F429I-Discovery_FW_V1.0.0\Projects\FW_upgrade\src\usb_bsp.c
PE1 (SDRAM NBL1) is NOT the over current pin, OTG_FS_OC is PC4 per the schematic #define HOST_OVRCURR_PORT GPIOE #define HOST_OVRCURR_LINE GPIO_Pin_1 #define HOST_OVRCURR_PORT_SOURCE GPIO_PortSourceGPIOE #define HOST_OVRCURR_PIN_SOURCE GPIO_PinSource1 #define HOST_OVRCURR_PORT_RCC RCC_APB2Periph_GPIOE #define HOST_OVRCURR_EXTI_LINE EXTI_Line1 #define HOST_OVRCURR_IRQn EXTI1_IRQn This is compounded elsewhere with an EXTI Interrupt Handler STM32F429I-Discovery_FW_V1.0.0\Projects\FW_upgrade\src\stm32f4xx_it.c Not sure any of this is used here, but it clearly came from somewhere else. Also the USE_ACCURATE_TIME makes assumptions about the TIMCLK being 72 MHz (6 * 12), which again needs more thought in the porting.2013-10-23 3:13 AM
Hi Clive1,
Thanks for all your valuable feedbacks on the STM32F429I-DISCO. They will be taken into account as soon as possible. Just to be precise for users fixing the issues by themselves waiting for official release: OTG_FS_OC is PC5. PC4 is the OTG_FS_PSO. Best Regards -Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.