2016-07-31 8:05 AM
Hi,
I am trying to drive 320x240 tft lcd with my stm32f429 mcu. I have connected all RGB and SYNC pins together with mcu and lcd but i can not see anything on the screen when i try to write something. I am not sure that i have configured the lcd parameters with the right values . The TFT lcd that i use is on the link below and you can see my lcd parameters that i configured it with cubemx.
TFT LCD datasheet:http://img.ozdisan.com/ETicaret_Dosya/412053_7958153.pdf
hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;
hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;
hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AH;
hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
hltdc.Init.HorizontalSync = 0;
hltdc.Init.VerticalSync = 0;
hltdc.Init.AccumulatedHBP = 70;
hltdc.Init.AccumulatedVBP = 13;
hltdc.Init.AccumulatedActiveW = 390;
hltdc.Init.AccumulatedActiveH = 253;
hltdc.Init.TotalWidth = 408;
hltdc.Init.TotalHeigh = 263;
hltdc.Init.Backcolor.Blue = 0;
hltdc.Init.Backcolor.Green = 0;
hltdc.Init.Backcolor.Red = 0;
HAL_LTDC_Init(&hltdc);
pLayerCfg.WindowX0 = 0;
pLayerCfg.WindowX1 = 0;
pLayerCfg.WindowY0 = 0;
pLayerCfg.WindowY1 = 0;
pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB888;
pLayerCfg.Alpha = 0;
pLayerCfg.Alpha0 = 0;
pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA;
pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA;
pLayerCfg.FBStartAdress = 0;
pLayerCfg.ImageWidth = 0;
pLayerCfg.ImageHeight = 0;
pLayerCfg.Backcolor.Blue = 0;
pLayerCfg.Backcolor.Green = 0;
pLayerCfg.Backcolor.Red = 0;
HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0);
pLayerCfg1.WindowX0 = 0;
pLayerCfg1.WindowX1 = 0;
pLayerCfg1.WindowY0 = 0;
pLayerCfg1.WindowY1 = 0;
pLayerCfg1.PixelFormat = LTDC_PIXEL_FORMAT_RGB888;
pLayerCfg1.Alpha = 0;
pLayerCfg1.Alpha0 = 0;
pLayerCfg1.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA;
pLayerCfg1.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA;
pLayerCfg1.FBStartAdress = 0;
pLayerCfg1.ImageWidth = 0;
pLayerCfg1.ImageHeight = 0;
pLayerCfg1.Backcolor.Blue = 0;
pLayerCfg1.Backcolor.Green = 0;
pLayerCfg1.Backcolor.Red = 0;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.