2016-01-23 5:24 AM
hello i want to use 4pin etm trace (ukink pro )on stm32f429
and i have this problem: if core clock > 100 mhz i cant use etm trace and if core clock<140 mhz i cant use ltdc is there any true configs for use etm trace on 180 mhz ? or how can i use ltdc in core clock <140 mhz? best regards2016-01-24 1:09 AM
I had to look up what LTDC is. It's a TFT interface.
In my experience LCD will work at lower clocks than nominal. If something claims it won't work below 140MHz, you might ''cheat'' and e.g. tell everything that you have a 16MHz external crystal while in fact you have a 8MHz one. Now the CPU will run at 90MHz, the LCD will refresh at 30Hz instead of 60Hz, but maybe the ETM might work....2016-01-24 3:45 AM
first of all thanks for your replay
yes I use tft lcd 8 inch (480*800 pixel) in RGB888 mode and my sdram is k4s561632c board crystal is 8mhz i self designed board with stm32f429IIT and have not any problem with ltdc peripherals(tft lcd) if core clock>140mhz . i check sdram by writing and reading value and check them in core clock lower than 140 mhz and i seen that every ting work correctly and i use const picture in flash of micro to show on lcd (without using sdram) and i seen that it work true on core clock <140mhz !!!!!!! but i cant used sdram and ltdc with each other in core clock <140 mhz , the lcd show is unclear best regardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.