2014-05-02 9:10 AM
Hi,
I am trying to implement firmware update on STM32F427 based custom board. I found that the STM32F427 has 1MB internal NOR flash. Where do I get the driver for it? Also, can someone provide a sample code to access low level driver functions using API(s)? #stm32-nor-flash-driver2014-05-02 9:41 AM
Hi
You do not have to worry about it being NOR Flash. Following the sequence in the reference manual for erasing and programming. '' Where do I get the driver for it? Also, can someone provide a sample code to access low level driver functions using API(s)? '' The Standard Peripheral Library has API interface for programming the Flash OR the STM32Cube should generate a similar API Both should be available from here https://my.st.com/st-extranet-web-active/active/catalog/tools/FM147/CL1794/SC961/SS1743/PF2579012014-05-02 11:10 AM
STM32F4xx_DSP_StdPeriph_Lib_V1.3.0\Project\STM32F4xx_StdPeriph_Examples\FLASH\FLASH_Program
Also a bunch of IAP examples. Search you part#, and look under ''Design Resources'' tabWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.