2018-04-20 5:47 AM
Hi all,
I'm using stm32f4 discovery with HAL drivers to realize a Synchronous BOOST DCDC.
When the system is turn on, the gpio PE8 and PE9 configured as PWM pins of TIM1,(in particular PWMOUT_CH1 & PWMOUT_CH1N) goes in SET state and for a few milliseconds keep the mos of the converter in ON state causing a little initial short circuit.
At startup PE8 and PE9 are in high impedance state?
If so,can i avoid this issue with a 100k pull down resistors?
There are software solutions to this problem?
Best regards
Bruno
2018-04-20 6:06 AM
>>There are software solutions to this problem?
Not on the F4 series, best to define default high-low states with external pull up/down resistors. Placing code to program the GPIO in the Reset_Handler can reduce the time they are in undesirable states as subsequent code will spin up clocks and PLLs.
I think one of the L4 or newer families provides a means of defining pin states at startup
2018-04-20 8:09 AM
Thanks Clive one
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.