2013-05-24 3:54 PM
Hi.
Please help. I write simple app using restricted KEIL to operate with AD5292 via SPI for my academic research project. To achive this I wrote the following code:int main(void)
{ /*!< At this stage the microcontroller clock setting is already configured to 168 MHz, this is done through SystemInit() function which is called from startup file (startup_stm32f4xx.s) before to branch to application main. To reconfigure the default setting of SystemInit() function, refer to system_stm32f4xx.c file */ GPIO_InitTypeDef GPIO_InitStruct; SPI_InitTypeDef spi; /*Enable or disable the AHB1 peripheral clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);//for SPI1 /** SPI1 GPIO Configuration PA15 ------> SPI1_NSS PB3 ------> SPI1_SCK PB4 ------> SPI1_MISO PB5 ------> SPI1_MOSI */ GPIO_StructInit(&GPIO_InitStruct); GPIO_InitStruct.GPIO_Pin = GPIO_Speed_50MHz; GPIO_InitStruct.GPIO_Pin = GPIO_Pin_15; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_OType = GPIO_OType_PP; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOA, GPIO_PinSource15, GPIO_AF_SPI1); GPIO_InitStruct.GPIO_Pin = GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5; GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOB, &GPIO_InitStruct); GPIO_PinAFConfig(GPIOB, GPIO_PinSource3, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOB, GPIO_PinSource4, GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOB, GPIO_PinSource5, GPIO_AF_SPI1); SPI_DeInit(SPI1); SPI_StructInit(&spi); spi.SPI_Direction = SPI_Direction_2Lines_FullDuplex; spi.SPI_Mode = SPI_Mode_Master; spi.SPI_NSS = SPI_NSS_Soft; spi.SPI_CPOL = SPI_CPOL_Low; //0 spi.SPI_CPHA = SPI_CPHA_2Edge; // 1 spi.SPI_DataSize = SPI_DataSize_16b; spi.SPI_FirstBit = SPI_FirstBit_MSB; spi.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64; SPI_Init(SPI1,&spi); SPI_CalculateCRC(SPI1,DISABLE); SPI_SSOutputCmd(SPI1, ENABLE); SPI_Cmd(SPI1, ENABLE); SPI_NSSInternalSoftwareConfig(SPI1, SPI_NSSInternalSoft_Set); while(1) { while(SPI_GetFlagStatus(SPI1, SPI_FLAG_TXE) == SET) ; SPI_SendData(SPI1, 0x93); while(SPI_GetFlagStatus(SPI1, SPI_FLAG_BSY) == SET) ; }}But I can't see any signaling at the pins. I tried to check if these pins weren't damaged. I wrote small app to toggle pins manually via GPIO functions. All worked fine.Thanks for any advices. #stm32f407vet6-spi1-pb3-pb4-pb52013-05-24 4:27 PM
RCC_APB1PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE);//for SPI1
APB2 APB2 ...2013-05-25 12:56 AM
Many thanks clive1 for your attention to my problem.
It was my mistake and if to say more precisely this was my misspell :) I tried many other variants before but without any success. :(I corrected ABP1 with ABP2 but I still can't see any signaling at the pins. And only when I switched the mode of the pins to GPIO and wrote the code to toggle states of the pins I can see meander at them.How do you think where can be the source of the problem?Thanks for your correction and help.2013-05-25 1:40 AM
Thanks a lot, clive1!
The second problem was at the following line:while(SPI_GetFlagStatus(SPI1, SPI_FLAG_TXE) == SET)
the line should bewhile(SPI_GetFlagStatus(SPI1, SPI_FLAG_TXE) == RESET)
Now everything is Ok.Many many thanks!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.