2014-05-12 12:29 AM
Dear all,
i am using STM32F405 with internal osc. clock. I connected a 3V lithium battery as VBAT, and would like to use the RTC to keep time when power is off. I read some samples here and there and implemented some RTC init / setup routines (finally using RTC_SetTime / RTC_SetDate). Until now, i can save time / date to RTC, but if i power off and on after 10 seconds, i see the time set as the same of power off (10 seconds old) while i was expecting the updated time. Every help is appreciated. Regards angelo2015-12-24 12:51 PM
Ai, I still can not fix the problem, time have pass for a few months now, my boss is after me. Any body can help? I will take some of my salary to pay you, otherwise I will lost my job. Please help.
2015-12-24 4:28 PM
Now might be a good time for you to clearly define what hardware you have built, and what aspects of its intrinsic functionality you have tested. ie does the LSE oscillate, can you measure the signal on a scope via the MCO, or other pin, and bench mark it against the HSE using the TIM connection internally. The correct functioning of the LSE oscillator is heavily dependent on the component choices, and wire lengths/layout. On DISCO boards the LSE is typically not populated, so components need to be added, and stub connections to pin headers disconnected.
Once we've addressed the basic functionality, then let's examine exactly what is and isn't working on the software side of things, and why that might be occurring.2015-12-25 4:45 AM
The hardware is done according the instruction:
X2, c23, c24, R53, R54 are populated, SB16 open, SB17 open. I even can not detect any signal in the X2 by using oscilloscope2015-12-25 6:08 AM
I also remove R52, connect +3V to pin 6 of STM32F429ZIT6, but didn't connect to pin 1 of STM32F103C8T6.
2015-12-25 6:42 AM
I don't know why need to open
SB16 , SB17 ? after open SB16 and S17, X2 connect to no where.
2015-12-25 6:57 AM
I don't know why need to open SB16 , SB17 ? after open SB16 and S17, X2 connect to no where.
So there aren't long stub traces to the P2 header, that's why, and the X2 pins then have short connections directly to the STM32, the connectivity is indicated in the schematic from the net names. ie PC14-OSC32_IN and PC15-OSC32_OUT Make sure you have the correct 32.768 KHz crystal, and it is correctly orientated. The LSE must explicitly be turned ON, make sure your code is doing this before you probe the pins. Ideally you want to measure the frequency using the internal TIM that's connected to the LSE/RTC source.2015-12-26 6:42 AM
Thanks a lot.
2015-12-26 1:31 PM
I still can not make the LSE work, I can not detect any signal from the crystal.
2015-12-26 3:13 PM
I still can not make the LSE work, I can not detect any signal from the crystal.
Unfortunately you're going have to get a lot more technically detailed on what suggestions you've tried, and the methods you've used to test and verify the components.2015-12-31 2:00 PM
I gave up to use crystal on board, I use external one from PC14, now program stop at backup SRAM.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.