2025-07-08 8:11 PM - last edited on 2025-07-09 1:22 AM by Andrew Neil
Hello,
I want to use the PB6 pin as an external interrupt input. When the PB6 pin is triggered, the program enters the low-power stop mode from the normal operation mode. When it is triggered again, the program enters the normal operation mode from the low-power stop mode. According to the above, the test found that after the program enters the low-power mode, it cannot return to the normal operation mode again.
Does anyone have experience in this area and can provide me with a solution?
Solved! Go to Solution.
2025-07-09 12:02 AM
@QSHAO.1 @TDK hello I configured PB6 as an external input interrupt. The configuration is as follows, and I am certain that this function is normal and effective.
EXTI_InitTypeDef EXTI_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOB, EXTI_PinSource6);
EXTI_InitStructure.EXTI_Line = EXTI_Line6;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4);
NVIC_InitStructure.NVIC_IRQChannel = EXTI9_5_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x03;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x03;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);And I placed the low-power mode in the time slice polling. Meanwhile, the PB6 pin is self-resetting and will only be triggered once at a time.
PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFI);
SystemInit();
2025-07-08 8:38 PM
Don't enter low-power mode from within an interrupt. Set a flag and do it in the main thread.
Additionally, if this is a button, you will probably have to debounce it.
2025-07-08 11:23 PM
Some information about how to exist stop mode (refer to RM0090), hope it's helpful.
If WFI or Return from ISR was used for entry:
Any EXTI lines configured in Interrupt mode (the corresponding EXTI
Interrupt vector must be enabled in the NVIC). The interrupt source can
be external interrupts or peripherals with wake-up capability.
If WFE was used for entry and SEVONPEND = 0
Any EXTI lines configured in event mode.
If WFE was used for entry and SEVONPEND = 1:
– Any EXTI lines configured in Interrupt mode (even if the corresponding
EXTI Interrupt vector is disabled in the NVIC). The interrupt source can
be an external interrupt or a peripheral with wake-up capability.
2025-07-09 12:02 AM
@QSHAO.1 @TDK hello I configured PB6 as an external input interrupt. The configuration is as follows, and I am certain that this function is normal and effective.
EXTI_InitTypeDef EXTI_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOB, EXTI_PinSource6);
EXTI_InitStructure.EXTI_Line = EXTI_Line6;
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_4);
NVIC_InitStructure.NVIC_IRQChannel = EXTI9_5_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x03;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x03;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);And I placed the low-power mode in the time slice polling. Meanwhile, the PB6 pin is self-resetting and will only be triggered once at a time.
PWR_EnterSTOPMode(PWR_Regulator_LowPower, PWR_STOPEntry_WFI);
SystemInit();
2025-07-09 8:21 AM
Show your full code.
2025-07-09 8:48 AM
Seems your code is normal and effective, then why you ask?
We ask where you start GPIO CLK, next why you call SystemInit after wake ? ETC.
2025-07-09 6:15 PM
@MM..1 According to the official data sheet, after exiting the stop mode, the system clock needs to be reset first.
Based on the current transformation, I was certain that entering the stop mode was effective, but when I wanted to exit the low-power mode again, the program did not run normally
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.