cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F401系列中,ADC_IN16通�?�和ADC_IN18通�?�是共用一个通�?��?�

L罗.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hi @LSL 罗​ and welcome to the Community :),

I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.  

Here is the translation of your post using Google translate:

In the STM32F401 series, do the ADC_IN16 channel and the ADC_IN18 channel share the same channel?

If I understand correctly, if you refer to the RM0368 and precisely Figure 38. Temperature sensor and VREFINT channel block diagram, you can conclude that you can output Vsense on both channel ADC1_IN16 and ADC1_IN18.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thank you

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
KDJEM.1
ST Employee

Hi @LSL 罗​ and welcome to the Community :),

I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.  

Here is the translation of your post using Google translate:

In the STM32F401 series, do the ADC_IN16 channel and the ADC_IN18 channel share the same channel?

If I understand correctly, if you refer to the RM0368 and precisely Figure 38. Temperature sensor and VREFINT channel block diagram, you can conclude that you can output Vsense on both channel ADC1_IN16 and ADC1_IN18.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Thank you

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.