2017-12-07 2:56 PM
Hi everyone,
I'm using one STM32F4 and I want to communicate with my LSM303 accelerometer. For that I'm using I2C, and just using I2C works fine but when I try to use DMA with it, it stops working.
When I use HAL_I2C_Master_Transmit_DMA it works and I got the IRQHandler. But when after that I want to use HAL_I2C_Master_Receive_DMA it says that the State of the I2C is not ready...
I read that the I2C was kind of messed up with the STM32FX but I don't understand why it's working fine without DMA.
Here's my I2C init :
void MX_I2C2_Init(void)
{
I2C_ST_INS.Instance = I2C2;
I2C_ST_INS.Init.ClockSpeed = 400000;
I2C_ST_INS.Init.DutyCycle = I2C_DUTYCYCLE_2;
I2C_ST_INS.Init.OwnAddress1 = 0;
I2C_ST_INS.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
I2C_ST_INS.Init.DualAddressMode = I2C_DUALADDRESS_DISABLED;
I2C_ST_INS.Init.OwnAddress2 = 0;
I2C_ST_INS.Init.GeneralCallMode = I2C_GENERALCALL_DISABLED;
I2C_ST_INS.Init.NoStretchMode = I2C_NOSTRETCH_DISABLED;
HAL_I2C_Init(&I2C_ST_INS);
}
void HAL_I2C_MspInit(I2C_HandleTypeDef* i2cHandle)
{
GPIO_InitTypeDef GPIO_InitStruct;
if(i2cHandle->Instance==I2C1)
{
//Not useful for this post
}
else if(i2cHandle->Instance==I2C2)
{
GPIO_InitStruct.Pin = MASTER_IMUB_I2C_SDA_Pin|MASTER_IMUB_I2C_SCL_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_I2C2;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
__HAL_RCC_I2C2_CLK_ENABLE();
/* DMA controller clock enable */
__HAL_RCC_DMA1_CLK_ENABLE();
hdma_i2c2_rx.Instance = DMA1_Stream2;
hdma_i2c2_rx.Init.Channel = DMA_CHANNEL_7;
hdma_i2c2_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_i2c2_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_i2c2_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_i2c2_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_i2c2_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_i2c2_rx.Init.Mode = DMA_NORMAL;
hdma_i2c2_rx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_i2c2_rx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_i2c2_rx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_i2c2_rx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_i2c2_rx.Init.PeriphBurst = DMA_PBURST_SINGLE;
if (HAL_DMA_Init(&hdma_i2c2_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(i2cHandle,hdmarx,hdma_i2c2_rx);
HAL_NVIC_SetPriority(DMA1_Stream2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream2_IRQn);
hdma_i2c2_tx.Instance = DMA1_Stream7;
hdma_i2c2_tx.Init.Channel = DMA_CHANNEL_7;
hdma_i2c2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_i2c2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_i2c2_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_i2c2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_i2c2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_i2c2_tx.Init.Mode = DMA_NORMAL;
hdma_i2c2_tx.Init.Priority = DMA_PRIORITY_VERY_HIGH;
hdma_i2c2_tx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;
hdma_i2c2_tx.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;
hdma_i2c2_tx.Init.MemBurst = DMA_MBURST_SINGLE;
hdma_i2c2_tx.Init.PeriphBurst = DMA_PBURST_SINGLE;
if (HAL_DMA_Init(&hdma_i2c2_tx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(i2cHandle,hdmatx,hdma_i2c2_tx);
HAL_NVIC_SetPriority(DMA1_Stream7_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(DMA1_Stream7_IRQn);
}
}
Do you have any ideas why it does not work when I'm using DMA with I2C ?
Thanks,
Victor
#i2c #stm32 #dma2017-12-07 3:10 PM
Also I forgot to mention that when it hits the callback I2C_DMAXferCplt for the Master_Transmit_DMA it says that the CurrentState of the I2C_HandleTypeDef is still equal to HAL_I2C_STATE_BUSY_TX and therefor it does not put the state back to READY. That why it does not receive anything when I call the Master_Receive_DMA.
Victor
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.