2015-07-24 6:18 PM
Hello
I have an STM32F429 discovery board
I program it with : STM32-Matlab/target (embedded target for Matlab and Simulink), STM32CubMx (configuration tool) and the toolchain: Keil uVision5 (lite).
I tray a very simple Simulink program, which consist of blinking a LED (PG13, green LED).
For this purpose, I used a ramp generator, from simulink sources, (period 1s, 5% ramle ratio).
The output of the generator is connected to the GPIO_Write block (pin PG13)
The GPIO pin 13 configuration is set as :
GPIO_Mode: OUT
GPIO_Speed : Low
type: pull up
when I download the code in the board, the LED is fired but it doesn't blink
what can I do to resolve this problem ?
thank you for your help
best regards
RCC_AHB1PeriphClockCmd
(
RCC_AHB1Periph_GPIOD
,
ENABLE
)
;
RCC_AHB1PeriphClockCmd
(
RCC_AHB1Periph_GPIOD
,
ENABLE
)
;
#!stm32f4-disco #gpio2015-07-24 6:34 PM
Look at the generated source code and step through it with the debugger?
2015-07-25 4:59 AM
Hello clive1
it seems to me, that the GPIO-clock enabling (validation) is not done.how can I enable the GPIO clock in the STM32CubeMx ?Tank's for the help2015-07-27 8:50 AM
Hi zaouche.khelil,
In order to confirm that issue is because of a missed clock enabling, please add ''__HAL_RCC_GPIOG_CLK_ENABLE();'' to your code.Let me know if this resolves the issue.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.