2012-02-24 3:36 AM
Hi all,
I'm searching to get work my UART4 port on my Discovery. I used the USART HyperTerminal_Interrupt example on stdPerif_example and I adapted to DISCOVERY. I see by some LedOn on the program that UART is working and sending interrupt. I manage to have a virtual USB-UART port with UM232R Ftdi but on my Putty nothing appeared I post my code /* USARTx configuration ------------------------------------------------------*/ /* USARTx configured as follow: - BaudRate = 9600 baud - Word Length = 8 Bits - Two Stop Bit - Odd parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled */ USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_2; USART_InitStructure.USART_Parity = USART_Parity_Odd; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; STM_EVAL_COMInit(&USART_InitStructure); Function void STM_EVAL_COMInit(USART_InitTypeDef* USART_InitStruct) { GPIO_InitTypeDef GPIO_InitStructure; /* Enable GPIO clock */ //RCC_AHB1PeriphClockCmd(UART4_TX_PIN | UART4_RX_PIN, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); //clock a PORTC RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE); //clock alla UART4! /* Connect PXx to USARTx_Tx*/ GPIO_PinAFConfig(GPIOC, GPIO_Pin_10, GPIO_AF_UART4); /* Connect PXx to USARTx_Rx*/ GPIO_PinAFConfig( GPIOC, GPIO_Pin_11, GPIO_AF_UART4); /* Configure USART Tx as alternate function */ GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Configure USART Rx as alternate function */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11; GPIO_Init(GPIOC, &GPIO_InitStructure); /* USART configuration */ USART_Init(UART4, USART_InitStruct); /* Enable USART */ USART_Cmd(UART4, ENABLE); } I also add void UART4_IRQHandler(void); to _it.h to manage interrupt _it.c void UART4_IRQHandler(void) { if(USART_GetITStatus(UART4, USART_IT_RXNE) != RESET) { GPIO_SetBits(GPIOD, GPIO_Pin_14); // accende led /* Read one byte from the receive data register */ RxBuffer[RxCounter++] = (USART_ReceiveData(UART4) & 0x7F); if(RxCounter == NbrOfDataToRead) { /* Disable the UART4 Receive interrupt */ USART_ITConfig(UART4, USART_IT_RXNE, DISABLE); } } if(USART_GetITStatus(UART4, USART_IT_TXE) != RESET) { GPIO_SetBits(GPIOD, GPIO_Pin_13); // accende led /* Write one byte to the transmit data register */ USART_SendData(UART4, TxBuffer[TxCounter++]); if(TxCounter == NbrOfDataToTransfer) { /* Disable the UART4 Transmit interrupt */ USART_ITConfig(UART4, USART_IT_TXE, DISABLE); } } } Where I'm failing? THanks #uart/usart-parity-and-wordlengt2012-02-24 4:07 AM
GPIO_PinAFConfig(GPIOC, GPIO_PinSource_10, GPIO_AF_UART4);
GPIO_PinAFConfig( GPIOC, GPIO_PinSource_11, GPIO_AF_UART4);2012-02-24 5:58 AM
YeP works!!!
Thanks clive1!!!! U save the daY!!! (to be precise is GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_UART4); GPIO_PinAFConfig( GPIOC, GPIO_PinSource11, GPIO_AF_UART4); without underscore) I see by Putty some data steam appearing but It's not the welcome message... uint8_t TxBuffer[] = ''\n\rUSART Hyperterminal Interrupts Example: USART-Hyperterminal\ communication using Interrupt\n\r''; Is the problem that DATA is uint16 and data uint8??void USART_SendData ( * USARTx,
uint16_t Data
)
or have I to configure putty in another way? That's what I see: à øüpÿÿà pÇüà à þüüà à ðüà à ðü~üà ü~à üüà Çà ü~Àüà à ðà ðüüüüüðüà üÿüü~üüà à þüà üpÿÿà pÇüà þüüà à ðüà à ðü~üà ü~à üüà üüüü~Çü~Çüüðü~üüüüüüà ü~à üü~øüÇà ü~ÿà üà Çà ü~Àüà à ðà ðüüüüà ø translation ISO-8859-1:1998 (Latin-1, West Europe) Thanks in advance2012-02-24 7:01 AM
Sorry working from memory. PinSource uses an index, Pin uses a mask.
You might want to check the ODD parity setting, that would give you weird characters if the terminal is configured for 8N1.2012-02-24 7:19 AM
no problem clive1 for pinsource
back to problem, If I try to send ''a'' (TXBuffer[]=''a'') the response to terminal is ü what's wrong? I double checked and my configuration is /* USARTx configured as follow: - BaudRate = 9600 baud - Word Length = 8 Bits - Two Stop Bit - Odd parity - Hardware flow control disabled (RTS and CTS signals) - Receive and transmit enabled I can't understand2012-02-24 7:40 AM
then if I send ''ab'' the response is
üpÀü ?2012-02-24 7:54 AM
If it's not the 8O2 rather than 8N1, then perhaps the baud rate is set up wrong.
Consider how the code is being compiled. The STM32F4-Discovery board has a different crystal speed for HSE than the library default. I think you want 8 MHz, not 25 MHz. Check the crystal speed in the IDE, and the value of HSE_VALUE2012-02-24 8:37 AM
thx clive1
I changed PLL_M value but the result is the same üpÀü @25Mhz üpÀü @8Mhz I don't know where else to look I'll send you my source files... I'll hope it's help.I'm using Atollic True Studio lite Thanks in advance ________________ Attachments : src.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I03h&d=%2Fa%2F0X0000000bTS%2F9M3pHzW3WhVxeYiORQ3mhfylrOfc0VakkGoJvC5nmSg&asPdf=false2012-02-24 7:54 PM
Well nothing looks to be hideously amiss, I guess at this point I'd be tempted to have it send a continuous stream of characters, 'U' being a particularly clever one, and measure/confirm the bit timing on a scope.
I might also try RealTerm, and try without parity.2012-02-27 2:23 AM
Dear Clive1,
I have performed the test you havesuggested
. I have tried with and without parity but nothing change... I post u some realTerm images (thanks for RT!!!) (->Can't upload images... I put on Attach) As u can see there is an ERROR bit! So I think that the problem is il my FTDI UM232r CHIP that can't handle the communication because the STM32 seems working good I post also a screenshot of PC10 pin of my oscilloscope I freeze the image of stream of U. It's seems work. The output values are: Vpeak-peak 3V Period 659us Freq 1,51 kHz baud= 8bit/2,5ms=3200 ( possible??) Is a problem that Vinput of 3V and not 3,3V for FTDI chip? Thanks again! ________________ Attachments : UART.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I06L&d=%2Fa%2F0X0000000bTR%2F4z5H.V7ZA3AXpr57yQVcV_eoJyBqQk1ZwbqBiyaMod4&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.