2012-07-23 10:53 AM
I got 2 new STM32F4 Discovery boards and both are not being recognized by STLINK utility. Here some of the observations. I compared the behavior to STM32F1 discovery board. (It is Windows 7 PC).
1) Plug in STM32F1 board. I see a pop up window saying USB mass storage device found.Plug in STM32F4. No window pops up.2) In STLink Utility I press the connect button. STM32F1 board is found and I can download program to flash. With STM32F4 I get a error message saying ''No STlink device found''My board has Rev Z devices. I tried the patch that was released to support Rev Z device. That did not work either.If we forget about programming the target device, I am not sure if the basic USB connection to the STLink is working. Any way to test/confirm this.Thanks #stm32f4discovery-stm32f42014-08-07 7:46 PM
Hi,
first of all, excuse my english. I have the same problem, plug in STM32F4, no window pops up. The preload demo is working, I use the mini USB connector.Any idea of what happens?Regards.2014-08-07 8:06 PM
And what version of Windows are we talking about? And what drivers have you installed?
2014-08-07 8:10 PM
Windows 7 - 32 bits. ST-Link/V2, Windows 7/Vista/XP (from ST's page)
2014-08-07 8:44 PM
not recognize the board, it's a normal behavior? I mean, when I connect the board to the PC does not recognize it as a new device.
2014-08-17 8:10 PM
Hello clive1,
Any suggestions / guidance on what else I can try?Regards.2014-08-18 4:16 AM
ISTR that you had to run the driver installer
before
you plug-in the board ?And that was on XP - I'd guess all this ''signed'' driver malarky on Win-7/8 just adds to the chance of it not working...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.