2015-05-19 2:52 PM
I am implementing a platform that must implement Datagram Transport Layer Security (DTLS).
I have the option of using the STM32F439x which includes Cryptographic Acceleration describbed in the datasheet as: ''Cryptographic acceleration: hardware acceleration for AES 128, 192, 256, Triple DES, HASH (MD5, SHA-1, SHA-2), and HMAC''It seems that the 'STM32 Cryptographic Library' uses this acceleration.Not being a security expert, I am having a hard time understanding if the Cryptographic Acceleration is useful for DTLS.Does anyone have experience in this?2015-05-20 1:57 AM
Implementing TLS or DTLS library from the scratch is useless (you WILL make bad security mistakes if your initials are not DJB), so the natural thing to do is to use a small, reputable, open source TLS/DTLS library. You have two options that I know of:
1.http://yassl.com/yaSSL/Home.html
(formerly CyaSSL) is a TLS library that supports DTLS and ithttp://yassl.com/yaSSL/cyassl-stm32.html
the hardware crypto facilities provided by the microcontroller that you mentioned. 2. The latest preview version of mbedTLS (formerly PolarSSL)https://tls.mbed.org/tech-updates/releases/mbedtls-1.4-dtls-preview-released
DTLS too, but I'm not sure if it supports STM32 hardware crypto.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.