cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F3Discovery SB13 and SB15 for VCP via USB ?

jjonethal
Associate II
Posted on November 02, 2015 at 21:15

Is there a way to use uart on stm32f103c8t6 for VCP over debugging chip or is there

a flash limitation for debugger firmware ? For Nucleo411 there is VCP support via STM32F103CBT6 which has twice as much flash as the debug chip on the f3discovery.

Any Ideas ?

Kind Regards Jean
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on November 02, 2015 at 22:09

Most DISCO boards don't support the VCP functionality.

The new STM32F469I-DISCO also has an STM32F103CBT6 and supports both the mbed and VCP functionality.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jjonethal
Associate II
Posted on November 03, 2015 at 09:18

Dear clive1,

Thank you for the fast response.

is it possible to flash the Stm32f3discovery debugger with the STM32F469I-DISCO debugger image ?

jjonethal
Associate II
Posted on November 05, 2015 at 15:16

I've tried to burn f2_4.bin from 411nucleo into the STM32F3Discovery board. After burning f2_4.bin Windows started to install the VCP driver but afterwards debugging was not possible. So i burned f2_1.bin and my debugger was alive again. I guess it's faster to use another open source alternative.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.