2013-03-20 4:23 PM
Hi,
I have a STM32F3Discovery eval. board which I used to build an IMU controlled by a computer through Graphical User Interface. This is an excellent board (9 Degrees of Freedom) and it is a good way to start.I have been curious about the Micro Framework from Microsoft but it requires at least 64KB of RAM. However the STM32F3 has only 48KB. Therefore, I decided to replace the current MCU with one that can fit the Micro Framework. I picked the STM32F407VGT6 for many reasons. One important reason is that it is entirely pin-compatible.I tried to download a demonstration code of the STM32F407VGT6 and I got a message telling:Fatal error: ST-Link, No MCU device found Session aborted!Failed to load flash loader
Things worked fine before I replaced the micro. The datasheet of the evaluation board says that the ST-Link can program any STM32 micro, so my change should work, right? What is the reason of the message?I am using IAR 6.50.1.4452 for ARM. #stm32f3discovery-stm32f407vg2013-03-20 5:31 PM
Things worked fine before I replaced the micro. The datasheet of the evaluation board says that the ST-Link can program any STM32 micro, so my change should work, right? What is the reason of the message?
Perhaps that you are shorting VCAP_1 to ground, and VCAP_2 isn't wired correctly either?2013-03-21 12:07 AM
Therefore, I decided to replace the current MCU with one that can fit the Micro Framework.
Instead of messing with the PCB, I would have used the STM32F4 Discovery, together with the MKI108V2 - there:
http://www.st.com/web/catalog/tools/FM116/SC1116/PF252687?s_searchtype=partnumber
This is essentially the same sensor combination, only on an external board.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.