2014-06-16 10:57 AM
2014-06-16 11:30 AM
Your #defines are what?
2014-06-16 11:40 AM
/* Enable GPIO clock */
RCC_AHBPeriphClockCmd(CAN_GPIO_CLK, ENABLE);
GPIO_DeInit(CAN_GPIO_PORT); //sarah, if you must, do it first, it'll break everything on the port
/* Connect CAN pins to AF7 */
GPIO_PinAFConfig(CAN_GPIO_PORT, CAN_RX_SOURCE, CAN_AF_PORT);
GPIO_PinAFConfig(CAN_GPIO_PORT, CAN_TX_SOURCE, CAN_AF_PORT);
/* Configure CAN RX and TX pins */
GPIO_InitStructure.GPIO_Pin = CAN_RX_PIN | CAN_TX_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(CAN_GPIO_PORT, &GPIO_InitStructure);
2014-06-16 4:04 PM
Hello clive1,
I really hoped you'd reply!! :)I saw you're the expert here.I already tried your configuration, but nothing happens.My defines are (sorry):/* Exported constants --------------------------------------------------------*/
//#define CANx CAN1
//#define CAN_CLK RCC_APB1Periph_CAN1
//#define CAN_RX_PIN GPIO_Pin_0
//#define CAN_TX_PIN GPIO_Pin_1
//#define CAN_GPIO_PORT GPIOD
//#define CAN_GPIO_CLK RCC_AHBPeriph_GPIOD
//#define CAN_AF_PORT GPIO_AF_7
//#define CAN_RX_SOURCE GPIO_PinSource0
//#define CAN_TX_SOURCE GPIO_PinSource1
#define CANx CAN1
#define CAN_CLK RCC_APB1Periph_CAN1
#define CAN_RX_PIN GPIO_Pin_11
#define CAN_TX_PIN GPIO_Pin_12
#define CAN_GPIO_PORT GPIOA
#define CAN_GPIO_CLK RCC_AHBPeriph_GPIOA
#define CAN_AF_PORT GPIO_AF_7
#define CAN_RX_SOURCE GPIO_PinSource11
#define CAN_TX_SOURCE GPIO_PinSource12
the commented out #defines are from the example, and the actual ones are to use the PA11-12 pins instead. Where am I doing wrong?2014-06-16 5:14 PM
#define CAN_AF_PORT GPIO_AF_9
It's not AF7 You have to pay attention to pin functions described in the Data Sheethttp://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/DM00046749.pdf
2014-06-16 5:17 PM
Hello clive1!!
After reading nearly every single post in the forum, I think I've found (part of) the solution:https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https%3a%2f%2fmy%2est%2ecom%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM32F3%20CAN%20Init&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews...basically to use PA11/12 pins I have to set GPIO_AF_9 instead of GPIO_AF_7.Now the CAN initialization DOES NOT fail, even if after that I have some problems in transmission. I'll check what's going wrong, hopefully it shouldn't take this long.Thanks a lot for you quick response!! :D2015-11-06 7:55 AM
Helo gaijingeek!
I have problem with stm32f373. I wrote a CAN application that works on the R8 (64k flash) version, but the RB (128k flash) and RC(256k) versions do not.I checked the alternate setups, CAN setups, etc...static void CAN_Config(void){ CAN_FilterConfTypeDef sFilterConfig; static CanTxMsgTypeDef TxMessage; static CanRxMsgTypeDef RxMessage; /*##-1- Configure the CAN peripheral #######################################*/ CanHandle.Instance = CANx; CanHandle.pTxMsg = &TxMessage; CanHandle.pRxMsg = &RxMessage; CanHandle.Init.TTCM = DISABLE; CanHandle.Init.ABOM = ENABLE; CanHandle.Init.AWUM = ENABLE; CanHandle.Init.NART = ENABLE; CanHandle.Init.RFLM = DISABLE; CanHandle.Init.TXFP = DISABLE; CanHandle.Init.Mode = CAN_MODE_NORMAL; CanHandle.Init.SJW = CAN_SJW_1TQ; CanHandle.Init.BS1 = CAN_BS1_8TQ; CanHandle.Init.BS2 = CAN_BS2_1TQ; CanHandle.Init.Prescaler = 2; if (HAL_CAN_Init(&CanHandle) != HAL_OK) { /* Initiliazation Error */ Error_Handler(); } /*##-2- Configure the CAN Filter ###########################################*/ sFilterConfig.FilterNumber = 0; sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK; sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT; sFilterConfig.FilterIdHigh = 0x0000; sFilterConfig.FilterIdLow = 0x0000; sFilterConfig.FilterMaskIdHigh = 0x0000; sFilterConfig.FilterMaskIdLow = 0x0000; sFilterConfig.FilterFIFOAssignment = 0; sFilterConfig.FilterActivation = ENABLE; sFilterConfig.BankNumber = 14; if (HAL_CAN_ConfigFilter(&CanHandle, &sFilterConfig) != HAL_OK) { /* Filter configuration Error */ Error_Handler(); } /*##-3- Configure Transmission process #####################################*/ CanHandle.pTxMsg->StdId = 0x321; CanHandle.pTxMsg->ExtId = 0x01; CanHandle.pTxMsg->RTR = CAN_RTR_DATA; CanHandle.pTxMsg->IDE = CAN_ID_STD; CanHandle.pTxMsg->DLC = 2;} ** * @brief CAN MSP Initialization * This function configures the hardware resources used in this example: * - Peripheral's clock enable * - Peripheral's GPIO Configuration * - NVIC configuration for DMA interrupt request enable * @param hcan: CAN handle pointer * @retval None */void HAL_CAN_MspInit(CAN_HandleTypeDef *hcan){ GPIO_InitTypeDef GPIO_InitStruct; /*##-1- Enable peripherals and GPIO Clocks #################################*/ /* CAN1 Periph clock enable */ CANx_CLK_ENABLE(); /* Enable GPIO clock ****************************************/ CANx_GPIO_CLK_ENABLE(); /*##-2- Configure peripheral GPIO ##########################################*/ /* CAN1 TX GPIO pin configuration */ GPIO_InitStruct.Pin = CANx_TX_PIN; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Alternate = CANx_TX_AF; HAL_GPIO_Init(CANx_TX_GPIO_PORT, &GPIO_InitStruct); /* CAN1 RX GPIO pin configuration */ GPIO_InitStruct.Pin = CANx_RX_PIN; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Alternate = CANx_RX_AF; HAL_GPIO_Init(CANx_RX_GPIO_PORT, &GPIO_InitStruct); /*##-3- Configure the NVIC #################################################*/ /* NVIC configuration for CAN1 Reception complete interrupt */ HAL_NVIC_SetPriority(CANx_RX_IRQn, 1, 0); HAL_NVIC_EnableIRQ(CANx_RX_IRQn);}/* Exported types ------------------------------------------------------------*//* Exported constants --------------------------------------------------------*//* User can use this section to tailor CANx instance used and associated resources *//* Definition for CANx clock resources */#define CANx CAN#define CANx_CLK_ENABLE() __CAN_CLK_ENABLE()#define CANx_GPIO_CLK_ENABLE() __GPIOB_CLK_ENABLE()#define CANx_FORCE_RESET() __CAN_FORCE_RESET()#define CANx_RELEASE_RESET() __CAN_RELEASE_RESET()/* Definition for USARTx Pins */#define CANx_TX_PIN GPIO_PIN_9#define CANx_TX_GPIO_PORT GPIOB#define CANx_TX_AF GPIO_AF9_CAN#define CANx_RX_PIN GPIO_PIN_8#define CANx_RX_GPIO_PORT GPIOB#define CANx_RX_AF GPIO_AF9_CAN/* Definition for USARTx's NVIC */#define CANx_RX_IRQn CAN_RX0_IRQn#define CANx_RX_IRQHandler CAN_RX0_IRQHandlerPlease help me.2015-11-06 8:29 AM
Check the vector table in startup.s, there may be additional IRQ Handlers, and different naming, double check those.
2015-11-08 11:08 PM
Hello clive1!
Thanks for the idea, but one-to-oneI compile the STM32Cube_FW_F3_V1.3.0\Projects\STM32373C_EVAL\Examples\CAN\CAN_Networking\project and the legacySTM32F37x_DSP_StdPeriph_Lib_V1.0.0\Project\STM32F37x_StdPeriph_Examples\CAN\CAN_Networking\ project. One does not work. Initialization error-free, I get an timeouterror when sending. I checked the startup fileand the vector table is the same as in the documentation.Use 64-foot version number, I use 64-foot version number, so I can not try the same project. ________________ Attachments : STM32Cube_FW_F3_V1.3.0.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0aW&d=%2Fa%2F0X0000000bdw%2FBoUlFDswv9EAZGMK0mNmprsrM8t2VupOWBVIf_h43D4&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.