2017-02-05 2:03 AM
I am use stm32f429.
Me need USB HS connection (speed 480 Mbit/sec) configured as 'Device_Only'.
Can I am C for this
application?
Or me need use external PHY ?
OTG not need me.
Thank you.
Solved! Go to Solution.
2017-02-06 12:08 AM
Can I am use internal PHY for this
application?
No. Internal PHY in STM32F429 is Full Speed only, for both USB modules. See STM32F429 datasheet, DocID024030 Rev 9, ch.3.34 Universal serial bus on-the-go high-speed (OTG_HS):
The USB OTG HS supports both full-speed and high-speed operations. It integrates the
transceivers for full-speed operation (12 MB/s) and features a UTMI low-pin interface (ULPI)for high-speed operation (480 MB/s). When using the USB OTG HS in HS mode, anexternal PHY device connected to the ULPI is required.JW
2017-02-05 5:39 AM
Hi. Your title has STM32F329 but working with STM32F4
See here:
https://community.st.com/0D50X00009Xke4ZSAR
Should be ok to use the internal USB PHY for USB HS. Also consider to source the STM32F429 Discovery board for quick testing of the sample code by ST.
2017-02-05 9:50 AM
Shall an integrated USB HS solution be needed in the future, STM32F72x might be the bext step
2017-02-05 9:34 PM
I am use stm32f429 really.
I am made mistake
in the message header. I am can not cerrect it.
Me need USB HS connection (speed 480 Mbit/sec) configured as 'Device_Only'.
Can I am use internal PHY for this
application?
Or me need use external PHY ?
OTG not need me.
Thank you.
2017-02-06 12:08 AM
Can I am use internal PHY for this
application?
No. Internal PHY in STM32F429 is Full Speed only, for both USB modules. See STM32F429 datasheet, DocID024030 Rev 9, ch.3.34 Universal serial bus on-the-go high-speed (OTG_HS):
The USB OTG HS supports both full-speed and high-speed operations. It integrates the
transceivers for full-speed operation (12 MB/s) and features a UTMI low-pin interface (ULPI)for high-speed operation (480 MB/s). When using the USB OTG HS in HS mode, anexternal PHY device connected to the ULPI is required.JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.