cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F303ze /Nucleof303ze adc siumltaneous triggering

DNYAR.1
Associate II

I need to have 2 adcs triggered simultaneously. Since i desire 3 differential inputs per ADC for the Nucleo F303zre board i can use ADC 1 and ADC3 .

STM32CuneIDE shows the Timer 20 trigger out event is available for both ADC triggering so i intend to use that for say a 1Msamples per second sampling rate.

  • Will using the same timer (e.g. timer 20) ensure both ADCs start at the same time?
  • Any examples for simultaneously triggering 2 ADC1 and ADC3 channels simultaneously?

Thanks

David

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
AScha.3
Super User

just set it as you like in Cube ,

for example : i use ADC1 + 2 and TIM8 , on F303 .

set adc trigger:


_legacyfs_online_stmicro_images_0693W00000bkzDaQAI.png

If you feel a post has answered your question, please click "Accept as Solution".

Hi AScha ,

So as i understand from you i will achieve the simultaneous sampling .

Thanks for your response. I have another question regarding using DMA but will make that another post.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.