2014-10-21 5:19 AM
Hello everyone, i am trying to start another timer with another timer update event. I tried to follow RM(see picture attached) and it seems that i did everything as it states, but maybe i understand something wrong, or i did something wrong. As i understand, Timer3 should be running and CNT register is incremented. When it reaches ARR value of TIM3, update event should be generated to trigger TIM2 and CEN bit should be 1 in TIM2->CR1. However TIM2 never starts. I'll be gratefull for any suggestions and comments. Code which i written for this is here;
#include ''stm32f30x.h''TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStructure;NVIC_InitTypeDef NVIC_InitStructure;GPIO_InitTypeDef GPIO_InitStructure;int i;void TIM3_IRQHandler(void){ GPIOE->ODR ^= GPIO_Pin_10; TIM_ClearITPendingBit(TIM3, TIM_IT_Update);// Clear interrupt pending bit, so it can go to interrupt again}int main(void){ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE, ENABLE); // GPIOE clock RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); // Port E pin 10 (blue LED) configuration GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOE, &GPIO_InitStructure); // NVIC structure NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); //Timer3 settings TIM_TimeBaseInitStructure.TIM_Period = 10000; // 0.1ms*10000 = 1s. Means counter will count to 10000 exactly 1s. TIM_TimeBaseInitStructure.TIM_Prescaler = 7200-1; // Divide clock freq. 72Mhz from 7200-1. so it gives ~ 0.1ms ticks. TIM_TimeBaseInitStructure.TIM_ClockDivision = TIM_CKD_DIV1; // Don't divide Timer clock frequency TIM_TimeBaseInitStructure.TIM_CounterMode = TIM_CounterMode_Up; // count from 0 to ARR value TIM_TimeBaseInit(TIM3, &TIM_TimeBaseInitStructure ); /* Configure Timer3 as a Master timner*/ TIM_SelectOutputTrigger(TIM3, TIM_TRGOSource_Update); // Timer 3 update event is selected as trigger output TIM_SelectMasterSlaveMode(TIM3, TIM_MasterSlaveMode_Enable); // synchronization between the current timer and its slaves (through TRGO) is enabled //Timer2 settings TIM_TimeBaseInitStructure.TIM_Period = 30000; // 0.1ms*30000 = 3s. Means counter will count to 30000 exactly 3s. TIM_TimeBaseInitStructure.TIM_Prescaler = 7200-1; // Divide clock freq. 72Mhz from 7200-1. so it gives ~ 0.1ms ticks. TIM_TimeBaseInitStructure.TIM_ClockDivision = TIM_CKD_DIV1; // Don't divide Timer clock frequency TIM_TimeBaseInitStructure.TIM_CounterMode = TIM_CounterMode_Up; // count from 0 to ARR value TIM_TimeBaseInit(TIM2, &TIM_TimeBaseInitStructure ); TIM_SelectInputTrigger(TIM2, TIM_TS_ITR0); // Timer 2 trigger source is TRGO0 TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Trigger); // The counter starts at a rising edge of the trigger TRGI // TIM_ClearFlag(TIM3, TIM_FLAG_Update); // Clear Timer3 UIF flag TIM_ITConfig(TIM3, TIM_IT_Update, ENABLE); // Enable Timer3 interrupts TIM_Cmd(TIM3, ENABLE); // Enable TIM3 counter while(1);}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.