2017-01-13 11:57 AM
STM32F3 Cube Drivers V1.7.0 is missing a few functions in the LL DMA Driver files. Specifically the 'LL_DMA_GetPeriphRequest' and 'LL_DMA_SetPeriphRequest'.
Is there some place I can download an older version and copy the functions?
2017-01-13 4:30 PM
Hello
Hebert.Reed
,I will check about your reported missingfunctions in the LL DMA Driver and I will getback to you as soon as possible.
However, you can download an old Cube version from
STM32CubeMx
(Click on Help->Install New Libraries
).Regards
Imen
2017-01-16 2:23 AM
Hello
Hebert.Reed
,'LL_DMA_GetPeriphRequest' and 'LL_DMA_SetPeriphRequest' functions are not implemented in the
STM32CubeF3 V1.6.0 and 1.7.0
(LL_DMA_SetPeriphRequest function is commented in the main file and it's not yet implemented)
Could you please checkm
aybe youare confusing
with another Cube drivers or
precise with more details the missing functions.
Regards
Imen
2017-01-16 10:55 AM
Thank you for taking the time to check into this for me. I have used the L4 LL Drivers previously and these functions are present there in order to assign the DMA channel to the DMA request. I was surprised that they weren't there in the F3 LL Drivers package.
Are you saying that they will be implemented in a future driver release? And in the mean time there are no LL Driver functions to do the same thing?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.