2015-08-03 6:34 AM
Hello!
I'm trying to use an STM32F3 to drive a gate driver for a class-D amplifier using sigma-delta modulation. Therefore I use the internal comparator to compare a reference signal with the actual integrated signal of the amplifier output. Depending on the comparator's output, the amplifier is switched on/off. Currently I'm using a timer interrupt at 1 MHz and check the comparator state within the interrupt routine. The routine is quite short but nonetheless the interrupt occurs quite often, limiting the capabilies of the µC. A D-flipflop with the comparator output as input, clocked by a 1MHz timer would also work, but an external component is required. Does anyone know another way to toggle an output depending on the comparator state with an update rate of 1 MHz? Thanks!2015-08-03 10:21 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.