2016-04-08 5:56 AM
Hallo.
I need to combine PGA and ADC for cases when the analog signal becomes very high or low.Is there an example how to do that?Additionally I would like to use one ADC for two synchronous signals by scanning two inputs. This is quite straight forward. However can I use one (!) PGA for one ADC sampling two inputs?Thanks, regards,Eduardo #adc-opamp-timer-controlled2016-04-08 6:13 AM
I think I have found it.
I need to connect the TIM1 CC6 Trigger to the OPAMP input MUX and use the same TIM1 as a trigger for the ADC. This will be tricky but I hope it will work.2016-04-08 6:28 AM
Now there is one problem.
I need to do two ADC conversions on one full MUX cycle of CC6. How can I configure this?Using sample on every edge is not good since the timing of the MUX and the ADC will then collide at 0/period!2016-04-11 9:50 AM
Hi deMier.Eduardo,
Refer to the OPAMP_PGA example in thehttp://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF260613
at this path STM32Cube_FW_F3_V1.4.0\Projects\STM32303C_EVAL\Examples\OPAMP\OPAMP_PGA -Hannibal-2016-04-12 4:44 AM
Hi Hannibal.
Thanks for the link. The example describes the simplest possible operation mode of the OPAMP as PGA.What I am looking for is using the OPAMP as PGA with- timer driven MUX toggling at the non-inverting input and - synchronous ADC-sampling at each (!) edge of the MUX switching timer signal.The techniques is often described as Ping Pong ADC Mode. It is used for sampling two analog channels (IQ) before processing the data with a complex FFT.This is far more complex than the example you provided. It would be great if you could look slightly deeper into this.Thanks. Regards.Eduardoedited: I have found a desciption of this technique in the RM0364 Reference manualSTM32F334xx advanced ARM®-based 32-bit MCUs in chapter 15.3.6 Timer controlled Multiplexer Mode of the OPAMP.Is there a running example somewhere? I don't mind if it is any other STM32 device.Thank you.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.