2020-07-05 1:06 PM
I am still having some issues with my STM32F334x8 and ADC DMA regular sequencing....
I am having ADC1 OVR flag set and am trying to use the IRQ which is successfully firing on IRQ but still need to understand how the sequencing and synchronization works with DMA a bit better.
OK, so seeing that DMA_CNDTRx is R/W, I can just write 7 to this register when disabled to reset that inside my OVR IRQ...
Now, how do I read or change the SEQ Sequence in the ADC1 peripheral to a known value ?
Does simply disabling the ADC and Re-enabling it reset the sequence count ? Would be nice to know where it is at but maybe that is not readable or writable ?
Solved! Go to Solution.
2020-07-05 11:14 PM
Figured it out.
Thank you to Eddie's STM32 videos for pointing out to me that the L[3:0] number if sequences to go through with a value of 0000 really means 1 (one) conversion !!!!
https://youtu.be/8lmujnLuJrQ?t=352
I had mistakenly thought that setting L[3:0] to 7 meant to sequence 7 registers and so it did NOT match the number of transfers programmed into DMA1 channel 1 and so that was why my DMA1 output array of ADC1 values did NOT appear in the same positions all the time. Reducing L[3:0] to 6 fixes this problem.
2020-07-05 11:14 PM
Figured it out.
Thank you to Eddie's STM32 videos for pointing out to me that the L[3:0] number if sequences to go through with a value of 0000 really means 1 (one) conversion !!!!
https://youtu.be/8lmujnLuJrQ?t=352
I had mistakenly thought that setting L[3:0] to 7 meant to sequence 7 registers and so it did NOT match the number of transfers programmed into DMA1 channel 1 and so that was why my DMA1 output array of ADC1 values did NOT appear in the same positions all the time. Reducing L[3:0] to 6 fixes this problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.