2015-03-14 8:33 PM
hi guy. I have a problem with accelerometter- gyroscope:
how to set address for accelerometter by I2C I need code communication with gyroscope A3G4250D thanhk you very much!2015-03-15 3:42 AM
can you explain the problem ?
The datasheet page 24 explain in detail the I2C slave address (SAD)2015-03-15 6:02 AM
sorry! I'm new member begin study.
I want to understand the method set address for slave on stm32f3discovery, but I don't understand: if I have one I2C master chip and have many slave (example sensor accelerometter share one I2C), how to set address for each slave, I have a question: do the address of slave have a default address2015-03-15 6:11 AM
Slave parts have fixed, default addresses, which are usually adequately unique/diverse to allow a system to use a lot of different devices. Refer to the manual for the slave parts, and if they have an address select pin to pick between one address, and others.
The 7-bit addressing is the high order bits, so some parts will refer to the address as say 0x25, the value programmed into the command request would be 0x4A. Look carefully at the diagrams in the part manual. The slave address is the first byte sent to the device, if a device on the bus recognizes the address it drives ACK low. At that point other devices stand down, or you determine no device with that address exists on the bus.2015-03-15 8:38 AM
I'll add another info:
The address of the accelerometer is in part modifiable because the last bit depends on the hihg/low value of the SDO pin.
This let you connect up to two device on the same I2C line with address11010001101001Other dvices can have three pind deidcated to adress configuration and allow you to conect up to eight components to same I2C each wiith is own address2015-03-15 9:06 AM
thank you everybody. I understood this problem!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.