2016-02-03 10:26 PM
I am getting ADC value on GPIOB Pin 1, using DMA, with continous conversion mode enable.
The ADC value that i obtain is > 4095, is this normal.Below is the table of adc value that i obtain compare to the real voltage connected to that pinReal voltage (V) Raw Value3.80 372163.97 390084.20 41216Why am i getting the raw value > 4095, is this behavior normal? i thought i should be getting 0 - 4095 (12 bit?)From the table above, i could deduce that my conversion from raw to real is / 100002016-02-03 10:45 PM
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
Or is it not ?
2016-02-03 10:56 PM
yes it is,
my settings are belowRCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.GPIO_Pin = BATTERY_VOLTAGE_PIN;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(BATTERY_VOLTAGE_PORT, &GPIO_InitStructure);
DMA_InitTypeDef DMA_InitStructure;
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&adc_value;
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 1;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStructure);
DMA_Cmd(DMA2_Stream0, ENABLE);
ADC_CommonInitTypeDef ADC_CommonInitStructure;
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div8;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_20Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
ADC_InitTypeDef ADC_InitStructure;
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = DISABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 1;
ADC_Init(ADC1, &ADC_InitStructure);
ADC_RegularChannelConfig(ADC1, ADC_Channel_9, 1, ADC_SampleTime_480Cycles);
ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
ADC_DMACmd(ADC1, ENABLE);
ADC_Cmd(ADC1, ENABLE);
ADC_SoftwareStartConv(ADC1);
2016-02-03 11:57 PM
And how is adc_value defined?
2016-02-04 12:08 AM
Back to your first post:
>Real voltage (V) Raw Value>
3.80
37216>
3.97
39008>
4.20
41216Are these the voltage on the GPIO/ADC pins ? Are you aware of the 3.6V specified limit for analogue inputs ?
2016-02-04 12:46 AM
I defined it as
volatile uint16_t adc_value;
and yes it is aware of the max voltage rating.
I found out the problem, that i dint include the line below
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
Once, i include it i could get the correct ADC value, but I dont understand why do i need to configure this settings, and is the meaning of
ADC_ExternalTrigConv_T1_CC1?
2016-02-04 3:15 AM
Perhaps because it stops random stack junk in the structure from misconfiguring the ADC. You've chosen continuous, and no trigger, but failing to initialize all fields appears to have resulted in a change of alignment.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.