2012-01-09 1:38 AM
Hi,
I've a problem with my STM32. I need to use fat filesystem on SD card to read/write/create files. I tried to use Chan FatFs module but it didn't working at all ... I use SD card in SDIO and 4 wires mode. When I debug, check_fs() function can't retrieve 0x55 0xAA on boot sector, but, when I read sector n�0 in the main(), I can correctly read all datas on boot sector. If someone can help me with this problem ... Thanks. #sdio-fatfs #sdio-chan-fatfs2012-05-30 8:54 AM
Hi,
I am trying to implement a SD logger. SDIO + FATFSI read a lot of threads on this forum as in others... in Frank blog.But I m till not able to make my STM32F405 working with chan-FSsource code.In the main.c, when I try to open a file,I have a similar issue as discribed delow.In check_fs(), it trys to read : if (disk_read(fs->drv, fs->win, sect, 1) != RES_OK) /* Load boot record */Then it enters the Default_Handler infinite loop...Any help would be very apreciated!!!PS : My IDE is eclipse.
2012-05-30 11:02 AM
fs->win - is that a pointer to or the buffer itself? Check if you maybe need &fs->win as a parameter of disk_read()
2012-05-31 1:39 AM
Hi,
Thanks for your advise.win is a pointer to the buffer win[xx]Thus I guess it is correct.I see that in fact the SD_WaitReadOperation() function stuck me.The processor receives an unexpected interrupt.I don t see what should be the issue.Maybe, it is a DMA issue...Do you have other ideas?Thanks in advanceGreg2012-05-31 2:46 AM
Hi,
Have a look at this thread ''Timing, DMA & SDIO ''Bug'' in Standards Peripherals Examples V3.5.0'' [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Timing, DMA SDIO Bug in Standards Peripherals Examples V3.5.0&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=161]here2012-05-31 8:44 AM
Thanks !!!
2012-10-16 9:45 PM
Hi,
I can't understand that why to use diskio.c to initialize the disk when we already have initialized sd card using low level sd_init() in sdio driver. Why can't we directly create a file on sd card using fileopen, read/write function? I have initialized SD card using SDIO peripheral......my next step is to save an image on sd card using FATfs..Please tell me how should i go now? Waiting for a prompt response2012-12-29 11:36 PM
Hi,
Does anyone have a solution? i am facing the same problem Thanks Michael2013-01-10 6:51 AM
Below an example based on FatFS:
STM32F2 and STM32F4 demonstration builder platform: http://www.st.com/internet/mcu/product/252146.jsp AN: http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/USER_MANUAL/DM00056717.pdf2013-03-05 1:48 AM
Hi
I am using the stm32f10b eval and i have to store a text file into a micro sd card connected to the stm32 with the spi protocol.I tried to use the fatfs but i found a problem when i used.so how i can integrate a fatfs ibrary to my project.thanks.2013-03-05 4:05 AM
Step 1 is to have some demonstrably functional SDIO sector/block read and write routines. These should be thoroughly tested, and you should inspect some of the card content.
Step 2 is to integrate these routines in DISKIO.C for the FatFs library. If you are having failures you'll need to be specific about what those are, and the errors generated, etc. One issue I've seen with GNU/GCC was a linker script that didn't zero the BSS section the required structures were allocated in.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.