2015-07-03 7:14 AM
Hi,
I am trying to program the discovery board using MATLAB+Simulink. Unfortunately the examples are not working on my board. I followed the simple example on Mathworks. I changed the pin to PG13, because on my board the LED is connected to this port. http://de.mathworks.com/help/supportpkg/stmicroelectronicsstm32f4discovery/examples/getting-started-with-embedded-coder-support-package-for-stmicroelectronics-stm32f4-discovery-board.html Everything compiles without an error. The program is downloaded to the board, but nothing happens. This is my board: http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/PF259090 Can anyone help me to get it working? Best Regards, Kai2015-11-20 5:19 AM
Anyone, who is interested in the official ST guide on ''Usage of STM32-MAT target'', there exist an Readme file.
It is hidden at file:///C:/MATLAB/STM32-MAT/STM32/Readme.html2015-12-03 12:31 AM
Is an update for the MATLAB-Target on the development roadmap?
''STM32 Embedded Target has been developped for MATLAB® R2014a version''(file:///C:/MATLAB/STM32-MAT/STM32/Readme.html)
2015-12-03 4:23 AM
Hi,
I wrote a step by step guide for myself on ''How to setup STM32-MAT/TARGET with MATLAB R2015a''. # # Software # - Windows 10 - MATLAB R2015a - Keil uVision V5.16.0 - STM32CubeMX V4.11.0 - STM32-MAT/TARGET 4.2.0 - git version 1.9.5.msysgit.1 # # Preparation # STM32 Embedded Target (STM32-MAT/TARGET) has been developped for MATLAB® R2014a version. There are some issues that have to be solved to get the STM32-MAT/TARGET working with MATLAB R2015a. 0. Install STM32-MAT/Target http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1533/PF258513 file:///C:/MATLAB/STM32-MAT/STM32/Readme.html see also file:///C:/MATLAB/STM32-MAT/STM32/html 1a. Local C Compiler Issue ''Changing line 67 in setup_for_lcc.m to the following line fixed the problem.'' args.mexOpts = rtwprivate('getMexCompilerInfo'); C:\Program Files\MATLAB\R2015a\toolbox\rtw\rtw\setup_for_lcc.m NOTE: You need to have administrative rights, when editing this file. 1b. Compiler Tool Chain Official answer from ST to fix this issue. See https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex%5fmx%5fstm32%2fSTM32F29I%20%2b%20MATLAB&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B Edit C:\MATLAB\STM32-MAT\STM32\rtw\stm32.tmf In Line 68 add ''COMPILER_TOOL_CHAIN = default'' 2. Create STM32CubeMX project The STM32CubeMX project (*.ioc) needs to be generated separately. It is not possible to create a new project from within MATLAB. Additionally the code neeeds to be generated once before using it with the STM32-MAT/TARGET. Just select ''Project > Generate Code''. 3. Configure Simulink Model There are two places where the preferences for the STM32-MAT/TARGET can be set. In Simulink: File > Simulink Preferences > Configuration Defaults > Code Generation Simulation > Model Configuration Parameters (Strg + E) > Code Generation 4. Create Simulink Model and Build Model Create a new Simulink Model, select ''STM32_Config'' from ''Target Support Package - STM32 Adapter/MCU_CONFIG'' and select the created STM32CubeMX from step 2. Clicking on ''Build Model'' will generate a Keil project, that can be ''build and run'' on the stm32 mircocontroller.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.