2014-09-22 8:44 AM
Hi,
I was working with Keil+ulinkpro on a custom board using an stm32f217 and everything was fine. I start working on some automated script for inital setup for our product using openocd. Somehow, it rendered the chip unresponsive. I am now unable to write/read with openocd and with keil/ulinkpro. I can see the SW device in the keil debugging tab.... I was wondering if there is a way to reset the MCU to it's initial state?Regards,Mart2014-09-24 12:44 PM
2014-09-24 1:06 PM
I'm not sure the ULink can nuke the options, you might try adding the ''STM32F4xx Flash Options'' region into the Settings->Flash Download->Programming Algorithm settings, and then mass-erase from there.
A stand-alone ST-LINK would offer all options provided by it's Utilities. If you have access to USART1/3 you could use the System Loader to wipe the read-out protection also. Haven't reviewed the HAL Flash code, the regular peripheral library wouldn't have set read-out protection with code similar to that presented.2014-09-24 1:31 PM
thanx for the Keil trick to mass erase. I can no wmake more testing and try to pinpoint the root cause of this mess.
thanx!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.