2017-05-22 1:59 AM
Hello,
I'm using STM32F207 with external USB-PHY in device mode.
I want to enter standby mode by SuspendCallback of USB. Because it is not possible to wakeup the STM32 by interrupt (ResumeCallback), I want to use the wakeup pin.
It is possible to use the output pin of external PHY (USB3300, signal D3) for wakeup?
Thanks,
Guenter
2017-05-22 2:07 AM
RM0033:
The microcontroller exits Standby mode when an external Reset (NRST pin), an IWDG
Reset, a rising edge on WKUP pin, an RTC alarm, a tamper event, or a time stamp event isdetected.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.