2017-01-05 11:19 PM
Hello,
i am using STM32F205RGT6 microcontroller i just want to run UART code.i just download the 'STM32Cube_FW_F2_V1.4.0' library and i don't modify any thing in this code.in this library i try with 'UART_Hyperterminal_IT' and 'UART_Printf' both but not works.but i am facing some problems.please try to solve my below query:1) when i run the UART code and observe on terminal i see the garbage values are printed.
i attached my code for your reference.
Any help in this will be appreciated more.
Thank You
Bhavin2017-01-06 8:36 AM
Hi
Maru.Bhavin
,I think your using your own PCB. So, please make sure that the your clock settings are aligned with the ones used in the examples.
'i try with '
UART_Hyperterminal_IT' and '
UART_Printf' both but not works.but i am facing some problems.
1) when i run the UART code and observe on terminal i see the garbage values are printed.'
-> For further investigation, please indicate
your Hyperterminal configuration:
data size
,
parity,
BaudRate...
And could you send me a screen shot of data displayed onthe Hyperterminal when you're using
'
UART_Hyperterminal_IT' or '
UART_Printf' examples.
Best regards,
Khouloud.
2017-01-06 11:57 AM
Does your board have a 25 MHz HSE crystal? Or an 8 MHz one? This alone would explain garbage data appearing on them terminal. as the data is coming out at the wrong speed.
Provide some more context about what exactly you are running it on, the CPU itself does not infer enough information.
2017-01-08 9:39 PM
Hi Clive One,
Thank you for your reply my board has ESA8.00000F20D25F(8 Mhz) crystal.
2017-01-08 10:00 PM
2017-01-08 11:15 PM
You need to make sure the PLL and HSE_VALUE reflect that it is using an 8 MHz clock and not 25 MHz, which is the default for the EVAL series boards.
2017-01-09 1:07 AM
Hi
Maru.Bhavin
,You should:
Regards,
Khouloud.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.