2013-01-20 7:00 PM
Dear All.
I use STM32F205RCT6 and want to use VCP of USB HS-Core (PB13-15) with embedded PHY.I wanted to use FS-Core (PA11-12) because I did and succeeded already.But 64pin device doesn't include FS-Core.I use VCP project of USB_Device_Examples in UsbLib V2.1.0.Descripters (VID,PID,SERIAL etc) are not changed (0x0483,0x5740,...).Then run the STM32, Connect to the WinXP 32bit by USB Cable.Failure the Device installation at first.But executing VCP_V1.3.1_Setup.exe installs driver,finally ' STMicroelectronics Virtual COM Port (COMxx) ' was appeared in Device manager without any warning.It can Open , Close , Tx , Rx , everything OK.Next , Connect to Win7 32bit by USB Cable,Failure the Device Installation at first.But executing VCP_V1.3.1_Setup.exe installs driver,finally ' STMicroelectronics Virtual COM Port (COMxx) ' was appeared in Device manager but with yellow warning (code 10).It can not Open the 'warning' port...Followings are declared in the project.USE_STDPERIPH_DRIVERUSE_USB_OTG_HSUSE_EMBEDDED_PHYIs it need to change the INF file FS-Core and HS-Core ?Could any one solve this ?Thanks2013-03-12 10:59 PM
Dear All.
Can I ask following again ?* CPU : STM32F205RCT6* Module : USB HS-Core (PB13-15) with embedded PHY.* Software : Virtual Comm Port of UsbLib V2.1.0.* OS : Windows 7 32bit* USB Driver : VCP_V1.3.1_Setup.exeMy result is that ' STMicroelectronics Virtual COM Port (COMxx) ' appears in Device manager WITH yellow warning (code 10).I can not open this port.Does anyone work well same as my condition ?Thanks
2013-04-04 2:01 AM
I solve this problem by changingCDC_IN_FRAME_INTERVAL to 0 in usbd_conf.h , and now all work fine. Also i use this fix
https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/DispForm.aspx?ID=24294
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.