2015-08-22 8:52 PM
I create a project with stm32cubemx last version , use osSignalSet and all osSignalXXX cause 'link error' 'notfound'
mcu :stm32F103C8T6(in cube ,this should be stm32f103c8tX) #stm32f1cube-rtos-bug2015-11-25 10:44 AM
I have the same problem with STM32CubeF3 v1.3.0. The osSignalSet, osSignalGet, osSignalClear, osSignalWait functions are defined in function prototypes but there is no code for these functions, therefore the link error. Look in cmsis_os.c to see whether the code is missing.
Because these functions are missing, I used osSemaphore functions instead.However I found that the return value of osSemaphoreWait() does not match the documentation. Look at the code to know what's really implemented.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.