2011-09-23 2:35 AM
Hello again,
This time with a problem in setting the times. I have a simple application that after the main call the SystemInit() function which set all the timers. This function is inside the system_stm32f10x.c file. Look at the code inside, I see: #define SYSCLK_FREQ_72MHz 72000000 #elif defined SYSCLK_FREQ_72MHz const uint32_t SystemFrequency = SYSCLK_FREQ_72MHz; /*!< System Clock Frequency (Core Clock) */ const uint32_t SystemFrequency_SysClk = SYSCLK_FREQ_72MHz; /*!< System clock */ const uint32_t SystemFrequency_AHBClk = SYSCLK_FREQ_72MHz; /*!< AHB System bus speed */ const uint32_t SystemFrequency_APB1Clk = (SYSCLK_FREQ_72MHz/2); /*!< APB Peripheral bus 1 (low) speed */ const uint32_t SystemFrequency_APB2Clk = SYSCLK_FREQ_72MHz; /*!< APB Peripheral bus 2 (high) speed */ and finally, the call to the SetSysClockTo72() function at the bottom of the file. In summary, after calling this function, the system clock should be set to 72MHz. If I call RCC_GetClocksFreq(&RCC_Clocks) just after callingSystemInit() and I use the debugger, I can see this numbers: SYSCLK_Frequency=4182367265 HCLK_Frequency=2124520693 PCLK1_Frequency=1051260827 The question is: shouldn't I see SYSCLK_Frequency equal to 72000000 or similar? and why these numbers in term s of billions and millions, as maximum 72? thanks for any help.2011-09-23 7:04 AM
Hi Pablo,
I have used STM3210C eval board and I have downloadeddemonstration firmware
code for this eval -IOExpander. At the beginning of code, they have called functionSystemInit(); from system_stm32f10x.c file. After this function, I have called functionRCC_GetClocksFreq(&RCC_Clocks); fromstm32f10x_rcc.c file. Before that I have defined RCC_Clocks strucure as RCC_ClocksTypeDef RCC_Clocks;. When I have looked with ST linkdebugger, everything seems fine to me, as you can see at attached picture.
Regards, Dragan ________________ Attachments : rcc_clocks.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0kY&d=%2Fa%2F0X0000000beZ%2FygTr4ElAyzH_rqXQZHwnZCxRfk4VvzyVsnu3nZ3tzIU&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.