2013-04-22 6:07 AM
STM32F103 has one CAN only. I want to send and receive data using the same CAN in normal mode(For testing purpose, CAN sends and receives message itself ). I have tried loopback mode and it worked fine. But when I configure CAN to normal mode it does not send or receive message at all over CAN. The CAN Tx pin is not showing CAN transmitted message on oscillioscope(In loopback it shows message correctly). Firstly I have used method described at
www.mikrocontroller.net/attachment/28831/siemens_AP2921.pdf
which tells a method to use CAN without transceiver using diodes. Then I thought may be this method is not working so I used a transceiver but I was unable to solve the problem. I am sure that it is not the software problem. What am I doing wrong?int main(void){ USART2_Config(); USART2_SendData_s(''Main Start:\n\r''); CAN_Config(); transmit_message(); while (1) { }}void CAN_Config(void){ // Enable GPIOA clock RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO , ENABLE); // CAN Periph clock enable RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1 , ENABLE); // GPIO CAN_RX Configuration GPIO_InitStructureCAN_RX.GPIO_Pin = GPIO_Pin_11; GPIO_InitStructureCAN_RX.GPIO_Mode = GPIO_Mode_IPU; GPIO_InitStructureCAN_RX.GPIO_Speed = GPIO_Speed_10MHz; GPIO_Init(GPIOA, &GPIO_InitStructureCAN_RX); // GPIO CAN_TX Configuration GPIO_InitStructureCAN_TX.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructureCAN_TX.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructureCAN_TX.GPIO_Speed = GPIO_Speed_10MHz; GPIO_Init(GPIOA, &GPIO_InitStructureCAN_TX); // CAN1 Filter,FIFO and Baudrate settings CAN_Struct_Init(); // CAN1 NVIC settings for FIFO 0 NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0); NVIC_InitStructure.NVIC_IRQChannel = USB_LP_CAN1_RX0_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x05; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // IT Configuration for CAN1 FIFO 0 message received interrupt CAN_ITConfig(CAN1, CAN_IT_FMP0, ENABLE); // Receive message initialized RxMessage.StdId = 0x00; RxMessage.ExtId = 0x00; RxMessage.IDE = CAN_ID_STD; RxMessage.DLC = 0; RxMessage.FMI = 0; for (i = 0; i < 8; i++) { RxMessage.Data[i] = 0; }}void CAN_Struct_Init(void){ // CAN1 register init CAN_DeInit(CAN1); CAN_StructInit(&CAN_InitStructure); // CAN1 cell init CAN_InitStructure.CAN_TTCM = DISABLE; // time-triggered communication mode = DISABLED CAN_InitStructure.CAN_ABOM = DISABLE; // automatic bus-off management mode = DISABLED CAN_InitStructure.CAN_AWUM = DISABLE; // automatic wake-up mode = DISABLED CAN_InitStructure.CAN_NART = DISABLE; // non-automatic retransmission mode = DISABLED CAN_InitStructure.CAN_RFLM = DISABLE; // receive FIFO locked mode = DISABLED CAN_InitStructure.CAN_TXFP = DISABLE; // transmit FIFO priority = DISABLED CAN_InitStructure.CAN_Mode = CAN_Mode_Normal; CAN_InitStructure.CAN_SJW = CAN_SJW_1tq; CAN_InitStructure.CAN_BS1 = CAN_BS1_2tq; CAN_InitStructure.CAN_BS2 = CAN_BS2_3tq; // CAN1 Baudrate = 250kbps (System clock and CAN clock is 24MHz) // CAN_Prescaler value= CAN_clock/(required_Baudrate*total_number_of_tq) // In present case, total_number_of_tq=CAN_SJW_1tq+CAN_BS1_2tq+CAN_BS2_3tq=6*tq // so CAN_Prescaler= 24MHz/(250kbps*6)=16 CAN_InitStructure.CAN_Prescaler = 16; if(CAN_Init(CAN1, &CAN_InitStructure)==CANINITOK) USART2_SendData_s(''Init OK:\n\r''); else USART2_SendData_s(''Init Fail:\n\r''); // CAN filter init CAN_FilterInitStructure.CAN_FilterNumber = 2; CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask; CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit; CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000; CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000; CAN_FilterInitStructure.CAN_FilterFIFOAssignment = CAN_FilterFIFO0; CAN_FilterInitStructure.CAN_FilterActivation = ENABLE; CAN_FilterInit(&CAN_FilterInitStructure); }void transmit_message(void){ Delay(0xffff);// Transmit message initialized
TxMessage.StdId=0x00; TxMessage.ExtId=0x00; TxMessage.RTR=CAN_RTR_DATA; TxMessage.IDE=CAN_ID_STD; TxMessage.DLC=5; TxMessage.Data[0]=0xA1; TxMessage.Data[1]=0xB2; TxMessage.Data[2]=0xC3; TxMessage.Data[3]=0xD4; TxMessage.Data[4]=0xE5; TransmitMailbox=CAN_Transmit(CAN1, &TxMessage); i = 0; while((CAN_TransmitStatus(CAN1, TransmitMailbox) != CANTXOK) && (i != 0xFFFF)) { i++; } USART2_SendData_s(''Succeed:\n\r'');}void USB_LP_CAN1_RX0_IRQHandler(void){ if(CAN_GetITStatus(CAN1, CAN_IT_FMP0) != RESET) { USART2_SendData_s(''CAN FIFO 0 IRQ:\n\r''); CAN_Receive(CAN1, CAN_FIFO0, &RxMessage); }} #can #can #stm32-can2013-04-22 6:50 AM
You can enable an internal loopback with:
CAN_InitStructure.CAN_Mode = CAN_Mode_Silent_LoopBack; // silent loopback mode, bus disconnect, debugging
2013-04-22 7:16 AM
Loopback and silent+loopback is working fine as expected.... I don't understand why it is not sending message in normal mode. Please guide!!
2013-04-22 8:05 AM
Send a continuous stream of messages.
Make sure USART1 isn't using flow control. Consider remapping CAN to PB8/9. (STM3210E-EVAL uses this) Get some boards with CAN designed on, experiment with them. Absent hardware review schematics. Known working hardware will avoid fighting your own issues. Make sure CAN transceivers are enabled. I used 125 kbps on the STM3210E CAN_InitStructure.CAN_TXFP = ENABLE;2013-04-22 12:11 PM
Do you have both nodes in normal mode and are both transceivers terminated? CAN won;t run in normal mode with just one node.
Jack Peacock2013-04-22 10:37 PM
please clarify Why at least two CANs must be used? I did not undersatnd why cannot I test one CAN alone in normal mode? I have tried one node system as well as two node system but using diode method(not transceivers as I have only one transceiver at this time so I have to shift my method to diodes as described preveously.)
2013-04-25 4:15 AM
I am still unable to figure out what is wrong with the normal mode of CAN. why is only loopback test works? In normal mode , CAN.Tx pin should response at least but it does not response at all. Please help out. I have also viewed several similar post for STM32F103 CAN normal mode problem but nobody have answered the issue. Is this problem is only with STM32F103 series?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.