2014-04-13 5:41 PM
Guys,
Can I use STM32F103VET6 with SDcard and uClinux? I put linux on SDcard and use internal RAM or I put linux on NAND flash ? Do I need external RAM ? Any ideas on doing that ? Thanks2014-04-13 8:50 PM
Have you worked with Linux or ucLinux kernels in the past?
With a minimal build of ucLinux how large is it? How large is a build with the feature set you need? What types of boards and memory configuration are people using with ucLinux? Do these seem to correlate with the resources provided by an STM32F103 running at 72 MHz?2014-04-13 11:03 PM
I worked with linux before..
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.