2010-03-29 5:20 AM
STM32F103VC and external SRAM
2011-05-17 4:45 AM
Also, I should have mentioned that I want to use FSMC.
2011-05-17 4:45 AM
This isn't a multiplexed device?
http://www.issi.com/pdf/61-64WV51216.pdf You'd need to set the STM32 up for PSRAM, with the byte lanes. Check the schematics provided for the STM3210E board http://www.st.com/stonline/books/pdf/docs/14220.pdf -Clive2011-05-17 4:45 AM
Thanks for your answer.
The evaluation board is based around the STM32F103ZET6 which has a lot more pins than mine, and therefore don't need the addres/data multiplexing.
The problem is that mine does not have enough pins for the adress bus, only eight.
So the question really is: How do I connect an external SRAM to the STM32F103VC, which does not have enough pins for the entire SRAM adress bus, using FSMC?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.