2014-10-21 2:29 AM
Hi,
i tried on my F103RB to create 4 Arrays with 512 entries and 3 byte wide.Should be calculated as 6144 byte. So i tried it to create but i only got Heap and Stack collision. Is there a possibility to move this arrays to the flash?I tried it with some section creating in linker script and defined the arrays with __ATTRIBUTE__ but i cannot figure it out.Here are the definitions of the arrays and the struct.#define WS2812_LED_MAX_ANZ 512WS2812_RGB_t WS2812_LED_BUF_CH1[WS2812_LED_MAX_ANZ];WS2812_RGB_t WS2812_LED_BUF_CH2[WS2812_LED_MAX_ANZ];WS2812_RGB_t WS2812_LED_BUF_CH3[WS2812_LED_MAX_ANZ];WS2812_RGB_t WS2812_LED_BUF_CH4[WS2812_LED_MAX_ANZ];typedef struct{ uint8_t red; // 0...255 (als PWM-Wert) uint8_t green; // 0...255 (als PWM-Wert) uint8_t blue; // 0...255 (als PWM-Wert)} WS2812_RGB_t;/opt/arm/bin/../lib/gcc/arm-none-eabi/4.6.1/../../../../arm-none-eabi/bin/ld: MagicLightController.elf section `.bss' will not fit in region `RAM'/opt/arm/bin/../lib/gcc/arm-none-eabi/4.6.1/../../../../arm-none-eabi/bin/ld: region `RAM' overflowed by 12932 bytesAnd here is the Linker Script im using. Without my section defines.Its in attached file2014-10-21 2:39 AM
Is there a possibility to move this arrays to the flash?
A declaration asconst
usually does fine, independant of the underlying toolchain. But you need to initializ eall required items, then. For example :WS2812_RGB_t WS2812_LED_BUF_CH1[WS2812_LED_MAX_ANZ] = {{R1,G1,B1},{...}, ... };
2014-10-21 2:51 AM
Ok, but const defines a constant and the array i fergot to describe is a array with fixed size but dynamic entries. So it wont work with const i think. But if i move this array to flash and the flash is not so often writeable as the ram. Humm i got too few RAM i think :(
2014-10-21 3:41 AM
Ok, but const defines a constant and the array i fergot to describe is a array with fixed size but dynamic entries. So it wont work with const i think.
It wouldn't work then, for sure. But that wasn't obvious from your initial post.Humm i got too few RAM i think :( Switching to a MCU with more RAM is an option. Have you checked the memory layout of your arrays ? Since each struct occupies 3 bytes, I expect the compiler to word-align it, wasting 1/4 of it's RAM size. Something like gcc's ''__attribute__(packed)
'' might help then.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.