2018-07-15 5:23 PM
Hi everyone, I am wondering if someone can help me, I want to make a device that uses the onboard USB VCP
on the STM32F103C8
I have set up using CubeMX an using keil
my problem is while the USB is connected to my PC... and the MPU's reset button is press I can no longer use my virtual com port
the only way I can get it working again is to disconnect the sub and plug it back in
has anybody got the code to make the USB do a soft disconnect when the MPU is soft reset
thank you
2018-07-16 12:19 AM
You are talking about a Nucleo board, with a ST-Link V2.1 ?
Are you sure it's not a problem on PC side ?
If you use a dumb terminal program that does not properly release the COM port, it could remain blocked until a reboot or removal (in case of an USB VCP).
2018-07-16 4:06 AM
hi, no i am not using a stlink, my programming is a ulink2
no i have tried connecting to the pc without connecting to a putty and terminal
but still when the press the restart button
i am using my own pcb, i am using the on chip USB
or is it better using one of the UART and USB to serial chips
2018-07-16 4:43 AM
Is VCP the same as CDC ?
on my machine Win10 using TeraTerm the USB CDC works well.Select any baud rate, without issue.
This COM4 is released when I press the Reset button.
and is re-established when I release Rest button most of the time, but not always.
However, TeraTerm usually doesn't work after a board reset.
I have to check the Device manager to see the COM4 is happy or not.
I have to press the Reset Button a few times and hold for a second or two then release..
then COM4 comes back in device manager and TeraTerm will see it again after you either exit TeraTerm or Select a different COM port and then go back to COM4, then TeraTerm will work again.
2018-07-16 8:24 AM
Then I'm not sure what VCP you speak about. A USB/VCP implementation on the target ?
Or some ulink functionality ?
2018-07-16 8:28 AM
to achieve a Virtual COM port on the PC, its our USB-CDC-device interface.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.