cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f103c8 - ADC1_2_IRQHandler not triggerd

Bogdan
Senior
Posted on January 29, 2017 at 21:04

Hello All

i have a timer which runs at 10 khz  and a adc channel in inject mode,  the problem is i have set some gpio toggling inside the ADC1_2_IRQHandler, but nothing happens.... 

I cant explain why the ADC1_2_IRQHandler is not being triggerd...

This is my adc init code ,  i am using stm32f10x_md.s file, but i see its defined the irq for adc as

DCD     ADC1_2_IRQHandler         ; ADC1 & ADC2

and in my project setings i have defined STM32F10X_MD   which coresponds in the stm32f10x.h file with bellow

#ifdef STM32F10X_MD

ADC1_2_IRQn = 18, /*!< ADC1 and ADC2 global Interrupt */      

NVIC_InitTypeDef NVIC_InitStructure;

GPIO_InitTypeDef GPIO_InitStructure;

ADC_InitTypeDef ADC_InitStructure;

DMA_InitTypeDef DMA_InitStructure;

NVIC_InitStructure.NVIC_IRQChannel = ADC1_2_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority =4 ;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 4;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_4 ;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;

GPIO_Init(GPIOA, &GPIO_InitStructure);

RCC_ADCCLKConfig(RCC_PCLK2_Div6); // ADC clock set to 72/6 = 12 MHZ

RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE);

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 |GPIO_Pin_11|GPIO_Pin_12;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_Init(GPIOB, &GPIO_InitStructure);

/* DMA1 channel1 configuration ----------------------------------------------*/

DMA_DeInit(DMA1_Channel1);

DMA_InitStructure.DMA_PeripheralBaseAddr = ADC1_DR_Address;

DMA_InitStructure.DMA_MemoryBaseAddr = (u32)&(myadcz[0]);

// Data direction: Peripheral is source

DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;

DMA_InitStructure.DMA_BufferSize = 8;

DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

DMA_InitStructure.DMA_Priority = DMA_Priority_High;

DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;

DMA_Init(DMA1_Channel1, &DMA_InitStructure);

DMA_ITConfig(DMA1_Channel1, DMA_IT_TC, ENABLE);

DMA_Cmd(DMA1_Channel1, ENABLE);

/* Put everything back to power-on defaults */

ADC_DeInit(ADC1);

/* ADC1 configuration ------------------------------------------------------*/

ADC_InitStructure.ADC_Mode = ADC_Mode_Independent;

ADC_InitStructure.ADC_ScanConvMode = ENABLE;

ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;

ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_None;

ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

ADC_InitStructure.ADC_NbrOfChannel = 1;

ADC_Init(ADC1, &ADC_InitStructure);

ADC_RegularChannelConfig(ADC1, ADC_Channel_5, 1, ADC_SampleTime_71Cycles5); //PA5 - Analog  channel 5

/* Enable ADC1 DMA */

//ADC_DMACmd(ADC1, ENABLE);

// INJECTED

/* Set injected sequencer length */

ADC_InjectedSequencerLengthConfig(ADC1, 1);

/* ADC1 injected channel Configuration */

ADC_InjectedChannelConfig(ADC1, ADC_Channel_4, 1, ADC_SampleTime_71Cycles5); //PA4 - Analog ADC1 - channel 4

/* ADC1 injected external trigger configuration */

ADC_ExternalTrigInjectedConvConfig(ADC1, ADC_ExternalTrigInjecConv_T1_TRGO);

ADC_ExternalTrigInjectedConvCmd(ADC1, ENABLE);

/* Enable JEOC interrupt */

ADC_ITConfig(ADC1, ADC_IT_JEOC, ENABLE);

/* Enable ADC1 */

ADC_Cmd(ADC1, ENABLE);

/* Enable ADC1 reset calibaration register */

ADC_ResetCalibration(ADC1);

/* Check the end of ADC1 reset calibration register */

while(ADC_GetResetCalibrationStatus(ADC1));

/* Start ADC1 calibaration */

ADC_StartCalibration(ADC1);

/* Check the end of ADC1 calibration */

while(ADC_GetCalibrationStatus(ADC1));

/* Start ADC1 Software Conversion */

ADC_SoftwareStartConvCmd(ADC1, ENABLE);

and my interrupt handler

void ADC1_2_IRQHandler(void)

{

GPIO_SetBits(GPIOB,GPIO_Pin_11);

voltage = ADC_GetInjectedConversionValue(ADC1, ADC_InjectedChannel_1);

/* Clear ADC1 JEOC pending interrupt bit */

ADC_ClearITPendingBit(ADC1, ADC_IT_JEOC);

GPIO_ResetBits(GPIOB,GPIO_Pin_11);

}

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
T J
Lead
Posted on January 29, 2017 at 21:52

are you using C++ ?

Can you put a break point in your code ?

I guess that ' void ADC1_2_IRQHandler(void)'

is not actually mapped into the linker.

can you find the original 'void ADC1_2_IRQHandler(void)' and put a break point in there too.

then you will know which one is being called.

if that is the problem then this could be your issue:

code needed to force linker to see your function.

extern 'C'  void ADC1_2_IRQHandler(void){

.

.

.

}

Posted on January 30, 2017 at 04:48

Do you handle/see the DMA interrupt?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on January 30, 2017 at 07:25

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6rL&d=%2Fa%2F0X0000000bwq%2FilFKnZvNfJjt2FD__2xPtF_0eQK_fw5mBwcpE8IxTIM&asPdf=false
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.