2015-07-30 8:55 AM
Hello
I have been trying to implement the VCP on a chip I am working on. I do not have any experience with USB and I just want to get this working so I can send some data to the device (will focus on USB later). I am using Eclipse + GCC and Cube for the initialising code. My PC recognizes the chip as COM port so far. Here's my code:nt main(int argc, char* argv[])
{
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
SystemClock_Config();
HAL_Init();
MX_USB_DEVICE_Init();
uint8_t data[] = ''Hello'';
HAL_Delay(1000);
// Infinite loop
while (1)
{
HAL_Delay(1000);
CDC_Transmit_FS(data, 5);
}
}
void MX_USB_DEVICE_Init(void)
{
/* Init Device Library,Add Supported Class and Start the library*/
USBD_Init(&hUsbDeviceFS, &FS_Desc, DEVICE_FS);
USBD_RegisterClass(&hUsbDeviceFS, &USBD_CDC);
USBD_CDC_RegisterInterface(&hUsbDeviceFS, &USBD_Interface_fops_FS);
USBD_Start(&hUsbDeviceFS);
}
However, when I call CDC_Transmit_FS(), I get a hard fault in the function USBD_CDC_SetTxBuffer(). The function CDC_Init_FS() is never called and the USBD_CDC_SetTxBuffer() function uses a variable that is never initialized. I saw a thread with a problem identical to mine at
/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/stackexchange
but I can't make it work. Thanks!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.