2023-11-12 10:13 PM
hello.
this is the first time I've had this problem , I describe this problem next:
1 the io initialization input is normal (this is the feature I want)
2 when I power off and restart, I find that the same pin initialization input is not responding
3 repeated power-off / power-on operation the pin initialization input sometimes does not respond
why does this happen, please tell me
thanks
2023-11-13 5:16 AM
Not sure what you mean by "io initialization input is normal", but:
1. Check if BOOT0 pin is at logic LOW (connected to GND directly or via resistor).
2. If there is a high-capacity capacitor (like 1000uF) in the power supply path, wait longer between power off and power on, or use Reset button.
2023-11-13 7:33 PM
thank you for your help
1. "io initialization input is normal" means that the pin function i want is the input function.
2. just like you said, BOOT0 pin is at logic Low
3.max capacitor of the power supply is 100uf
thanks
2023-11-14 12:12 AM
Hi @shan chen ,
Please share your minimal project, not only the main file (if possible the .ioc file). So the members of the community and us can help you.
2023-11-14 5:45 PM
thank you for your help
sorry, i tried many times, the .ioc file transfer failed
do you have any suggestions about the problems I mentioned or have you encountered similar problems before
best wishes
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.