2013-04-27 12:49 PM
Hi All,
I've rummaged through the archives but didn't really see what I'm looking for here. We have a few PWM power control designs based on the Atmel ATTINY861A which provides fairly complete support for this application space. However we're limited by its flash capacity and 8-bit architecture. I've been looking at both the F100 and F103 STM32 devices and was hoping someone who has dug into the functional limitations and quirks of these devices may be able to offer some insight. Specifically it appears the F100 may offer support of more PWM channels compared to the F103, but I believe the F103 can support at least three independent complimentary PWM channels with deadtime control. And if I read correctly both devices support hardware PWM cycle termination and A/D synchronized to PWM cycle. However the 3X clock speed of the F103 is well worth the price bump assuming we're not foregoing any power application specific functionality which may be unique to the F100. Aside from that any cautions on functionality loss and/or restriction specific to power control applications with the lower pin count packages (32,48) relative to 64 LQFP versions? Thanks, -mm #stm32f100-stm32f103-pwm-control #motor-cntl2013-04-29 7:02 AM
I think that the best STM32 for Power Control is the STM32F30X. 4x5MSPS ADC + 2*144MHZ Motor PWM + 4xPGA + 7xCOMP. And it is a Cortex-M4 with floating point.
2013-04-29 8:52 AM
Focus here on our review for potential use of F0 for BLDC motor control - one small subset of your, ''Power Control.'' This for professional (for profit) applications.
Required MCU capability: Pins Function Ana 6 PWM ''pair'' w/deadband & hw shutdown No 3 Hall sensor in No 3/6 Analog comparator (1 or 2) Yes 3 Normal control inputs: run, direction, brake No 4 SPI (accommodate client specific add ons) No 9 ADC: speed, torque, motor V, bemf(3), i-lmt(3) Yes 1 PWM Fault-In pin No 29/32 GPIO/ADC req'd With the use of SPI - inevitable extra ADC and GPIO ICs can be accommodated. Analog comparators are, ''life-savers'' - available ex-MCU via tiny sot 23-5 pack. The 48 pin QFP package ''just fits'' in several of our designs - raising the appeal of F0...2013-04-29 12:29 PM
Analog comparators are, ''life-savers'' - available ex-MCU via tiny sot 23-5 pack.
These are handy indeed, IMO it's the most missing thing in F1 series.
You can emulate it with ADC but it may be somewhat slow.
2013-04-29 2:03 PM
''These are handy indeed, IMO it's the most missing thing in F1 series.
You can emulate it with ADC but it may be somewhat slow.''
We're on same page here. We employ these for ''cycle by cycle'' current limiting - and indeed are order of magnitude faster than ADC - and run w/out concern of SW hang. Regulatory agencies love this ''independence''as it greatly aids safety. And - if HW properly married to SW - such current measurement/limiting can be made fully interactive - clearing automatically as the fault passes. (ideal to prevent nuisance ''trips.'')Analog comparators are, ''life-savers'' - available ex-MCU via tiny sot 23-5 pack.
These are handy indeed, IMO it's the most missing thing in F1 series.
You can emulate it with ADC but it may be somewhat slow.
2013-04-29 3:19 PM
my method:
start with the fastest, must memory, most I/O member of the family (in your case f1x) if t can do it, continue, else find another family. then start seeing which lesser members f that family can handle your app. it is a definite time waster not6 to verify with the biggest, baddest member of the family first. Start high, go down Erik2013-04-30 9:07 AM
Would have thought that something here earned some response from originator...
Now - meaning no disrespect to Erik (clearly he's helped many) wish to present, ''the rest/other side of the story...'' Suspect that the application's demands don't register high enough in your, ''biggest/baddest'' guideline! Certainly - if cadillac part cannot satisfy - chevy has almost no chance... But wait - having worked in design/sales/legal (engineering then law school) hi-tech - have too often observed that ''desperate - resource restricted'' - someway/somehow ''find a way'' - missed (most always - not properly or ''even'' considered) by ''deeper pockets'' approach. And have observed this effect to extend into device selection - as well. So ''biggest/baddest'' often only ''best'' if effort/focus/imagination/experience retain that level. Frequently - they do not! Anecdotal - but does demonstrate - our group recently chose an MCU due to its inclusion of analog comparator. (thought vital) And later discovered (to our horror) that 2 were needed. (now what?) Lesson learned - employ the MCU for that which it alone is best equipped - offload other functions to secondary devices - provided cost/size is w/in reason/bounds... Time to market, competitive posture, price target, availability, development tools and on-going support (and future product development) all should receive scrutiny - and ''biggest/baddest'' may stumble under such weight. (our findings) How does the cost to ''design down'' compare against cost to, ''design up?'' Perhaps worthy of consideration - one size/method ''fits all'' - but likely is never optimal...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.