2016-06-13 11:32 AM
Hi, I have evidence that the UART embedded bootloader of the STM32F070CBT6 does not work. Is this expected ? I have tried the boot sequence with other STM32 variants for years, and I cannot find any written explanation on why the embedded UART bootloader simply does not work for this particular uC type. Is STM32 aware of this ?
2016-06-13 11:53 AM
You'll need to pull the manufacturing/productions codes marked on the top of the device to better isolate the specific part/batch you are having issues with.
Can you access the device via the SWD port, and in other mode is it functioning normally?What is the BOOTn setting in the Option Bytes?The System Loader will be sensitive to transitions on any other pins/interfaces it might expect to see communications on. Refer to the documented list of pins for the device.2016-06-14 7:29 AM
Hiquintero.francisco,
First, I recommend you to take a look to the , p 43 to see th recommendation about bootloader use within you device. AS mentionned, if the HSI is used and its clock not enough accurate,the bootloader might not function correctly. So, try use the HSE as clock source, or see about HSI calibration as done in this . Come back to tell if this solve your problem. -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.