2017-06-01 8:49 PM
Hi all,
I used the STM32F051's ADC function. If I Enable the Auto-off mode (AUTOFF), in the power-off state, the calibration value that produced from HAL_ADCEx_Calibration_Start() will be deleted ?
#stm32f051 #stm32-adc2017-06-08 6:46 AM
Hi
Wu.Tung_Chang
,Based on RM0091:
As ADC power is not removed by ADEN bit nor the auto-off mode, once calibration was done, auto-off mode does not require re-calibration.
But during the time (auto-off enabled), if the STM32F051 MCU enters the standby mode, supply voltage will be removed from VDD/VDDA connected to ADC. So calibration will be required.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.