cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F042 MEM_MODE problem

x8932
Associate II
Posted on September 30, 2015 at 16:59

Hello,

i use STM32F042C6 MCU and change SYSCFG MEM_MODE to 1 (System Flash memory mapped at 0x00000000) but always see Main Flash (0x08000000) data from address 0x00000000.

Also i try set 11 (Embedded SRAM mapped at 0x00000000) but unsuccess.

Also i try jump to system bootloader (0x1FFFC400) but MCU back to 0x08000000 vector after small delay (with USB connected).

Can anybody use software jump to system bootloader ?

#stm32f0
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on September 30, 2015 at 17:25

Hi Mitek,

It seems that you haven't update the BOOT0 pin (it has to be set to 1).

Did you tried using the ST-Link Utility?

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.