2017-07-24 9:41 PM
Hello friends, I am using
STM32F030RCT6 (ARM 32-bit Cortex-M0)
in my design. I want to make use of the in-built Real-time clock (RTC) from the Chip. Where should I connect the battery, i.e., between which pin numbers? Can someone help me in this regard? Thanks in advance.2017-07-25 10:03 AM
Dear
cgovind.raj
,If you have a battery to keep RTC working while main VDD is off, You need to select his cousin STM32F091RC : You will see VBAT pin at position 1 in this LQFP64 package. For value line series F030 we are not selling neither full testing the VBAT mode. It has a smll extra cost $. ☺.
Cheers,
STOne -32
2017-07-25 4:00 PM
Might well also need an LSE crystal, check what's powered in the low power domain.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.