2020-06-16 7:33 AM
There isn't any PC14 PC15. Is it really inaxessible on this MCU and I'm have to find suitable HSE crystal in order to get high-presition RTC?
Solved! Go to Solution.
2020-06-16 7:51 AM
Hello MBelk,
Pins PC14 and PC15 are indeed not present on the TSSOP20 version of the STM32F030. As such, you cannot add an external low-speed oscillator. You can still use the internal low-speed clock (LSI) as a source for the RTC, although the achieved accuracy won't be as high as when using an external low-speed clock.
2020-06-16 7:51 AM
Hello MBelk,
Pins PC14 and PC15 are indeed not present on the TSSOP20 version of the STM32F030. As such, you cannot add an external low-speed oscillator. You can still use the internal low-speed clock (LSI) as a source for the RTC, although the achieved accuracy won't be as high as when using an external low-speed clock.
2020-06-16 8:18 AM
Yes, but 4.096 MHs standard HSE crystal resonator will helps.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.